AM243x MCU+ SDK  09.02.00

Detailed Description

Header that prefixes all TISCI messages sent via secure transport.

Parameters
integ_checkThis field should always be initialized to zero on GP devices. The mechanism to calculate the integrity check for HS devices is under definition.
rsvdReserved field for future use. Initialize to zero.

Data Fields

uint16_t integ_check
 
uint16_t rsvd
 

Field Documentation

◆ integ_check

uint16_t tisci_sec_header::integ_check

◆ rsvd

uint16_t tisci_sec_header::rsvd