AM243x MCU+ SDK  09.02.00
Bind unibase to a specific platform

Introduction

Files

file  unibase_binding.h
 functions to bind unibase to a specific platform
 

Functions

int ubb_memory_out_init (char *mem, int size)
 initialize the internal memory_out function More...
 
int ubb_memory_out_close (void)
 de-initialize memory_out function More...
 
char * ubb_memory_out_buffer (void)
 return the memory pointer of memory_out More...
 
int ubb_memory_out_lastline (char **str, int *size)
 return the most recent output line in memory_out More...
 
int ubb_memory_out_alldata (char **rstr, int *size)
 return the all written line data in the buffer More...
 
int ubb_memory_file_out (const char *fname)
 write the data in memory_out buffer into a file More...
 
void ubb_default_initpara (unibase_init_para_t *init_para)
 return the default initialization parameters supported in the binding layer More...
 
void ubb_set_gptp_gettime64 (get64ts_t func)
 set gptptime function for ub_gptp_gettime64 More...
 
void ubb_unibase_easyinit (void)
 initialize unibase with 'ubb_default_initpara' More...
 

Typedefs

typedef uint64_t(* get64ts_t) (void)
 

Macros

#define UBB_DEFAULT_DEBUG_LOG_MEMORY   (64*1024)
 ubb_memory_out_init uses this value to allocate internal buffer when 'mem' parameter is NULL. More...
 
#define UBB_MEMOUT_ENDMARK   "---###---"
 ubb_memory_out always add this end mark at the end of printing. More...
 
#define UBB_DEFAULT_LOG_INITSTR   "4,ubase:45"
 ubb_default_initpara uses this string as 'ub_log_initstr' More...
 
#define UBB_GETENV   getenv
 get a string from an environment variable More...
 

Macro Definition Documentation

◆ UBB_DEFAULT_DEBUG_LOG_MEMORY

#define UBB_DEFAULT_DEBUG_LOG_MEMORY   (64*1024)

ubb_memory_out_init uses this value to allocate internal buffer when 'mem' parameter is NULL.

◆ UBB_MEMOUT_ENDMARK

#define UBB_MEMOUT_ENDMARK   "---###---"

ubb_memory_out always add this end mark at the end of printing.

◆ UBB_DEFAULT_LOG_INITSTR

#define UBB_DEFAULT_LOG_INITSTR   "4,ubase:45"

ubb_default_initpara uses this string as 'ub_log_initstr'

◆ UBB_GETENV

#define UBB_GETENV   getenv

get a string from an environment variable

Typedef Documentation

◆ get64ts_t

typedef uint64_t(* get64ts_t) (void)

Function Documentation

◆ ubb_memory_out_init()

int ubb_memory_out_init ( char *  mem,
int  size 
)

initialize the internal memory_out function

Parameters
memuse this memory as a buffer for memory_out. if mem is NULL, allocate memory internally for 'size' bytes
sizesize of memory to be used for memory_out
Returns
0 on success, -1 on error
Note
if this is not explicitly called, it is called internally with mem=NULL and size=UBB_DEFAULT_DEBUG_LOG_MEMORY

◆ ubb_memory_out_close()

int ubb_memory_out_close ( void  )

de-initialize memory_out function

Returns
0 on success, -1 on error
Note
this must be called whichever case of the explicit call or the internal call of 'ubb_memory_out_init'

◆ ubb_memory_out_buffer()

char* ubb_memory_out_buffer ( void  )

return the memory pointer of memory_out

Returns
memory pointer

◆ ubb_memory_out_lastline()

int ubb_memory_out_lastline ( char **  str,
int *  size 
)

return the most recent output line in memory_out

Parameters
strpointer of string pointer to return result string
sizepointer of integer pointer to return result size
Returns
0 on success, -1 on error

◆ ubb_memory_out_alldata()

int ubb_memory_out_alldata ( char **  rstr,
int *  size 
)

return the all written line data in the buffer

Parameters
rstrallocated pointer of the returned data
sizesize of the returned data
Returns
0 on success, -1 on error
Note
returned pointer in *str must be freed by the caller. the allocation size is the same as the size in ubb_memory_out_init

◆ ubb_memory_file_out()

int ubb_memory_file_out ( const char *  fname)

write the data in memory_out buffer into a file

Parameters
fnamefile name
Returns
0 on success, -1 on error

◆ ubb_default_initpara()

void ubb_default_initpara ( unibase_init_para_t init_para)

return the default initialization parameters supported in the binding layer

Parameters
init_parapointer of unibase initialization parameter

◆ ubb_set_gptp_gettime64()

void ubb_set_gptp_gettime64 ( get64ts_t  func)

set gptptime function for ub_gptp_gettime64

Parameters
funca function which returns 64-bit gptp time

◆ ubb_unibase_easyinit()

void ubb_unibase_easyinit ( void  )

initialize unibase with 'ubb_default_initpara'

Note
ubb_memory_out is initialize with no memory. To use memory logging, 'ubb_memory_out_init' needs to be called separately