AM243x INDUSTRIAL COMMUNICATIONS SDK  09.02.00
ICSS_EMAC_Attrs Struct Reference

Data Fields

uint8_t emacMode
 
uint32_t phyAddr [ICSS_EMAC_MAX_PORTS_PER_INSTANCE]
 
uint8_t phyToMacInterfaceMode
 
uint8_t halfDuplexEnable
 
uint8_t enableIntrPacing
 
uint8_t intrPacingMode
 
uint16_t pacingThreshold
 
uint8_t ethPrioQueue
 
uint8_t learningEnable
 
uint8_t portMask
 
uint8_t txInterruptEnable
 
uint32_t linkIntNum
 
uint32_t rxIntNum
 
uint32_t txIntNum
 
uint32_t l3OcmcBaseAddr
 
uint32_t l3OcmcSize
 
uint32_t linkTaskPriority
 
uint32_t rxTaskPriority
 
uint32_t txTaskPriority
 
uint32_t splitQueue
 

Field Documentation

◆ emacMode

uint8_t ICSS_EMAC_Attrs::emacMode

Mode from ICSS_EMAC_Modes

◆ phyAddr

uint32_t ICSS_EMAC_Attrs::phyAddr[ICSS_EMAC_MAX_PORTS_PER_INSTANCE]

Phy address of the ports. For mac mode, phyAddr[0] is used. For switch mode, phyAddr[0] and phyAddr[1] are used.

◆ phyToMacInterfaceMode

uint8_t ICSS_EMAC_Attrs::phyToMacInterfaceMode

PHY to MAC Interface Mode Valid values : ICSS_EMAC_PhyToMacInterfaceModes

◆ halfDuplexEnable

uint8_t ICSS_EMAC_Attrs::halfDuplexEnable

Flag to enable Half duplex capability. Firmware support also is required to enable the functionality. Valid values : 0 to disable, 1 to enable.

◆ enableIntrPacing

uint8_t ICSS_EMAC_Attrs::enableIntrPacing

Flag to enable Interrupt pacing. Valid values : ICSS_EMAC_InterruptPacingConfig

◆ intrPacingMode

uint8_t ICSS_EMAC_Attrs::intrPacingMode

Pacing mode to be used. Valid values : ICSS_EMAC_InterruptPacingModes

◆ pacingThreshold

uint16_t ICSS_EMAC_Attrs::pacingThreshold

Number of packets threshold for Pacing Mode1

◆ ethPrioQueue

uint8_t ICSS_EMAC_Attrs::ethPrioQueue

Queue Priority separation for RT and NRT packets. If packets are in Queue <= ethPrioQueue, they will be forwarded to RT callback and others to NRT callback

◆ learningEnable

uint8_t ICSS_EMAC_Attrs::learningEnable

Flag to enable learning. Not applicable for Mac mode. Valid values : ICSS_EMAC_LearningModes

◆ portMask

uint8_t ICSS_EMAC_Attrs::portMask

Port Mask. Indication to LLD which ports to be used Valid values: ICSS_EMAC_MODE_SWITCH, ICSS_EMAC_MODE_MAC1, ICSS_EMAC_MODE_MAC2

◆ txInterruptEnable

uint8_t ICSS_EMAC_Attrs::txInterruptEnable

Flag to enable TX Interrupt. Valid values : 0 to disable, 1 to enable. If this flag is enabled, ICSS_EMAC_txInterruptHandler() is registered as ISR for the txIntNum interrupt. This interrupt handler unblocks ICSS_EMAC_osTxTaskFnc() and calls the user-specified txCallback.

◆ linkIntNum

uint32_t ICSS_EMAC_Attrs::linkIntNum

◆ rxIntNum

uint32_t ICSS_EMAC_Attrs::rxIntNum

◆ txIntNum

uint32_t ICSS_EMAC_Attrs::txIntNum

◆ l3OcmcBaseAddr

uint32_t ICSS_EMAC_Attrs::l3OcmcBaseAddr

L3 OCMC Base Address

◆ l3OcmcSize

uint32_t ICSS_EMAC_Attrs::l3OcmcSize

L3 OCMC Size

◆ linkTaskPriority

uint32_t ICSS_EMAC_Attrs::linkTaskPriority

Link Task Priority

◆ rxTaskPriority

uint32_t ICSS_EMAC_Attrs::rxTaskPriority

RX Task Priority

◆ txTaskPriority

uint32_t ICSS_EMAC_Attrs::txTaskPriority

TX Task Priority. Valid only if txInterruptEnable is set to 1

◆ splitQueue

uint32_t ICSS_EMAC_Attrs::splitQueue

Flag to be set for using split Queue i.e. seperate queue for each of ports