- Attention
- This release version includes experimental support for integration of alternate PHY components. Introduced in version 1.07.00. Please see the note on Experimental Features.
Overview
The Software Development Kit (SDK) for EtherCAT allows you to quickly integrate EtherCAT slave functionality into your device. The SDK is supported for Sitara processors by Texas Instruments Incorporated and currently available for AM64x and AM243x series of Cortex®-R5 based devices.
This document collection contains a Quickstart Guide, the User Manual, and the API Reference Manual for the EtherCAT Slave SDK. The API consists of the following modules: an API to access the basic EtherCAT Slave functionality, the API for the CiA 402 (Drives and Motion Control), the cyclic buffer handling API, and a board support package API.
Licensing
Copyright © 2023, KUNBUS GmbH
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
-
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
-
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
-
Neither the name of the copyright holder nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Release Version 2.00.01
New Features:
-
[OSS1-3262] Migration to Industrial communications SDK 9.02.00.49
Also containing support for:
-
CCS 12.7.0
-
SysConfig 1.20.0
-
TI Clang 3.2.2
-
OSAL 1.2.1
-
HWAL 2.0.1
-
[OSS1-3251] Access to PDO entry size in PDO mapping change callback function
-
PDO entry size change triggers the PDO mapping change callback.
Release Version 2.00.00
New Features:
-
[OSS1-2390] Ethernet over EtherCAT EoE
Major changes:
-
Open API to implement third party TCP/IP Stacks.
-
Example provided for AM64x-EVM on Linux SDK.
-
Simple example mailbox size incremented to 1024 bytes.
-
[OSS1-2697] CoE complete access API updated
-
The API functions used for object complete access now have subIndex as parameter.
-
Only subIndex values 0 and 1 are valid.
-
[OSS1-2911] Update ESI files
-
Tested with EtherCAT Conformance Test Tool 2.5.0.
-
Added missing content.
-
Replaced all tabs by spaces.
-
[OSS1-2603] Allow applications without RX or TX Process Data
-
Input or output SyncManagers are not configured if RX or TX PDOs are not present.
-
[OSS1-2934] Remove base data types in the reserved index area
-
Data types from index 0x0260 till 0x07FF are removed.
-
Data type OCTET_STRING can be used instead of removed data type ARRAY_OF_SINT.
-
Data type UNICODE_STRING can be used instead of removed data type ARRAY_OF_INT.
-
[OSS1-2906] Support mapping of objects larger than 30 Bytes
-
Objects larger than 30 Bytes can be mapped now to the process data.
-
The documentation has been extended with more detailed information.
-
[OSS1-2966] Integration of Industrial communications SDK 9.02.00
Also containing support for:
-
CCS 12.6.0
-
SysConfig 1.19.0
-
TI Clang 3.2.1
-
OSAL 1.2.0
-
HWAL 2.0.0
-
[OSS1-3067] Integrate NVM library for persistent data storage
-
EtherCAT examples updated with NVM library.
-
EtherCAT examples now use EEPROM and not Flash memory to store EtherCAT EEPROM data.
-
[OSS1-1043] File access over EtherCAT FoE
-
Demo supports the file transfer over EtherCAT
-
FoE APIs use NVM library to access the FoE data
-
The documentation has been extended with a new page for FOE.
Bugfixes:
-
[OSS1-2841] Disabled PDOs can't increase process data length
-
If a PDO is disabled, then the process data length is not updated.
Release Version 1.99.00
New Features:
-
[OSS1-1678] Refactoring of EtherCAT API
Major changes:
-
All functions return uint32_t as error code
-
All functions use API handle as first parameter
-
API split in categorized header files
-
Signature changes documented on API Changes
-
[OSS1-1533] Fix CiA402 mode change problem
Switching between drive modes (torque mode, velocity mode, position mode) that crashed the example application has been fixed.
-
[OSS1-2241] Fix CiA402 velocity mode
If the target position was set to zero, the application was not performing any operation mode (csp, csv or cst).
Release Version 1.13.00
Bugfixes:
-
[OSS1-1476] Fix customer ssc
missing diag file compile for customer ssc did cause linker error on customer compiled libs.
-
[OSS1-1302] Integration of Industrial communications SDK 9.00.00.01 Also containing support for:
-
CCS 12.4
-
SysConfig 1.17.0
-
TI Clang 2.1.3
-
OSAL 1.01.01
-
HWAL 1.00.06
-
[OSS1-613] Upgrade to OSAL 1.1
Fixed warnings and corrected inconsistencies between function names and arguments.
-
[OSS1-586] Bool and bit type objects in process data mapping.
The process data offsets for types smaller than a byte has been fixed.
-
[OSS1-594] Fix record object names.
The composed string for record objects is properly configured when: subIndexes are registered in an unsorted manner.
no subIndexes registered between two of them.
-
[OSS1-596] Record entries registered in an unsorted manner are now shown correctly.
New Features:
-
[OSS1-1302] Update to TI Industrial Communications SDK 9.0.
Integration into new SDK deployment structure of TI.
-
[OSS1-609] Integrate A53 -> R5F FBTL support.
-
[OSS1-597] Optimize record object configuration time.
-
[OSS1-633] Implement enumeration types in CoE Object Dictionary.
Enumeration types now can be created and used in combination with variable, array and record objects.
-
[OSS1-615] Configure max subIndexes for SyncManager.
SyncManager subIndex count is now freely configurable.
-
[OSS1-601] Signature change for EtherCAT state machine callbacks.
Callbacks must return uint16_t value instead of EC_API_SLV_EUserRetCodes_t.
uint16_t values must be AL Status codes defined in the stack.
-
[OSS-613] Upgrade to OSAL 1.1
Fixed warnings and corrected inconsistencies between function names and arguments.
-
[OSS-586] Bool and bit type objects in process data mapping.
The process data offsets for types smaller than a byte has been fixed.
-
[OSS-609] Integrate A53 -> R5F FBTL support.
Simple and CTT demo did pass conformance tests.
ul> [OSS-597] Optimize record object configuration time. /ul>
-
[OSS-633] Implement enumeration types in CoE Object Dictionary.
Enumeration types now can be created and used in combination with variable, array and record objects.
-
[OSS-615] Configure max subIndexes for SyncManager.
SyncManager subIndex count is now freely configurable.
-
[OSS-601] Signature change for EtherCAT state machine callbacks.
Callbacks must return uint16_t value instead of EC_API_SLV_EUserRetCodes_t.
uint16_t values must be AL Status codes defined in the stack.
Release Version 1.12.02
New Features:
-
[OSS1-211] Add support for MCU+ SDK 08.06.00.22.
Release Version 1.12.01
-
[P2101-89] Add support for FBTL over UART. For testing purposes and prove of concept FBTL over UART line is added.
Release Version 1.12.00
New Features:
-
[DTKEC-1333] Add API to load custom PRU firmware from application.
-
[DTKEC-1184] Diagnosis history object 0x10F3 is now supported.
New API implemented to enable the diagnosis object and to send diagnosis messages.
Bugfixes:
-
[DTKEC-1286] Correct duplicated error class entries EC_API_eERR_DEPRECATED, EC_API_eERR_GROUP_TYPE_NOT_SET
The error entries previous contained the same ID. This has been corrected:
-
EC_API_eERR_GROUP_TYPE_NOT_SET: 0x0039
-
EC_API_eERR_DEPRECATED: 0x003A
-
[DTKEC-1295] Fix cppcheck usage
-
[DTKEC-1289] Add error code for object index below manufacturer specific area (0x2000)
for these functions:
-
EC_API_SLV_CoE_odAddVariable
-
EC_API_SLV_CoE_odAddArray
-
EC_API_SLV_CoE_odAddRecord
-
[DTKEC-1290] EC_API_SLV_PDO_createEntry returns an error code if an object without PDO mapping flag
or incompatible flag is mapped to a PDO:
-
EC_API_eERR_INVALID if object does not contain OBJACCESS_TXPDOMAPPING or OBJACCESS_RXPDOMAPPING flags.
-
EC_API_eERR_INVALID if PDO is RX type and object contains only OBJACCESS_TXPDOMAPPING flag.
-
EC_API_eERR_INVALID if PDO is TX type and object contains only OBJACCESS_RXPDOMAPPING flag.
-
[DTKEC-1345] Increase mailbox maximum size from 256 to 1024 Bytes.
-
[DTKEC-1270] Start and Stop output handler callbacks fixed for 2 CPU solution.
-
[DTKEC-1060] Array and Record objects with 255 subIndex never return from function.
Release Version 1.11.00
New Features:
-
[DTKEC-1251] Add support for mdio manual mode workaround
-
[DTKEC-1214] Refactor EC_API_SLV_setState function.
Added error code parameter to inform about an application error.
-
[DTKEC-1088] Support for MCU+ SDK 8.05.00.01
-
[OSAL-315] Support for CCS 12.1 and SysCfg 1.14. (OSAL)
-
[OSAL-256] Support for CCS 12.1 and SysCfg 1.14. (HWAL)
-
[OSAL-257] OSAL V 1.00.09.
-
[OSAL-270] HWAL V 1.00.03.
Improved license detection speed
-
[OSAL-315] Support MCU+ SDK 8.04.00.17.
Release Version 1.10.01
New Features:
-
[DTKEC-1191] Documentation improvements
Changed placement of EtherCAT logo to top of documentation, grammatical corrections and minor formatting changes.
Release Version 1.10.00
New Features:
-
[OSAL-254] Support for CCS 12 and SysCfg 1.13. (OSAL)
-
[OSAL-256] Support for CCS 12 and SysCfg 1.13. (HWAL)
-
[OSAL-257] OSAL V 1.00.07.
-
[OSAL-270] HWAL V 1.00.01.
Improved license detection speed
Bugfixes:
-
[DTKEC-339] F030h object description is corrupted after setting SubIdx 0 RW flag.
F030h Object appears to be corrupted after calling the service DPR_eService_EC_CoESubIdx0WrFlag
which sets the subIndex 0 with RW flag. By default array subIndex 0 flags use to be RO. This has been corrected
Release Version 1.09.00
New Features:
-
[OSAL-218] Support for MCU+ SDK 8.04.00.01.
-
[DTKEC-900] Added new tools for improved code quality.
Extended existing and added static code analysis tools as well as automated additional tests in CI environment.
Bugfixes:
-
[DTKEC-840] Custom PHY Lib iterators caused data abort
Custom PHY lib list handler did not properly check length of the list. This has been corrected.
-
[OSAL-218] Invalid PHY reset pins on AM243x LP
Fixed syscfg error on Launchpad PHY reset lines (exchanged).
Release Version 1.08.00
New Features:
-
[DTKEC-956] Support for MCU+ SDK 8.03.00.05.
Bugfixes:
-
[DTKEC-852] Beckhoff Stack 5.13 fix bitmaps in ESI file
-
[DTKEC-933] Fix timeout issue on eval version.
On specific circumstance eval limit was expired before expected.
-
[DTKEC-893] Register permission tests failing with 1.7.0 release
Fix RegPerm set value where Bitwise or was logical or (by error)
Release Version 1.07.00
New Features:
-
[DTKEC-839] Add TI logo to ESI files
Replaced generic logo icon in ESI with TI icon.
-
[DTKEC-825] Integrate Timesync Router configuration
Added static Timesync Router configuration to DTK (PRU Integration).
-
[DTKEC-823] PRU/MDIO clock frequency change
PRU/MDIO clock frequency increased to 333MHz to improve performance.
-
[DTKEC-822] Add support for MCU+ SDK 8.3.x
Add SDK 8.3 basic support with experimental enhancement of PRU/MDIO API.
-
[DTKEC-824] Use newly created PRU firmware from changed path
-
[DTKEC-752] Minor documentation changes
Minor changes in the documentation: corrected formatting in known issues, replace DTK with SDK, corrected link to FAQ.
-
[DTKEC-744] Customer Slave Sample Code (SSC) for Windows and Linux Operating Systems
In ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_slave/stack/patch there are a new makefile.custom-ssc and readme.md. Please follow the instructions in the readme.md to build your own SSC library from the available sources by ETG.
-
[DTKEC-453] Integrate Beckhoff Stack 5.13
Customer Slave Sample Code (SSC) is compiled using Beckhoff Stack sources with a patch applied. Both patch and build process were adapted to the recently released SSC_V5i13.
-
[OSAL-148] OSAL revision 1.0.3
Feature: new OSAL revision supporting MCU+ SDK 8.03.xx
Bugfixes:
-
[DTKEC-792] Hotfix custom SSC
Some flags on custom built Beckhoff library have been missing blocking status/error LEDs and DC from working on customer created libbkhfSsc.a.
-
[DTKEC-748] Second Vendor ID is set in custom SSC
Second vendor id was still shown on valid Beckhoff SSC compile.
Experimental Features
- Attention
-
Features listed below are early versions and should be considered as "experimental".
-
Users can evaluate the feature, however the feature is not fully tested at TI side.
-
TI would not support these feature on public e2e.
-
Experimental features will be enabled with limited examples and SW modules.
-
[DTKEC-773] Custom PHY interface provided by stack.
For evaluation hardware an example implementation is provided for DP83869.
Release Version 1.06.01
New Features:
-
[DTKEC-693] Build SSC Library with EC patch standalone
Provide a patch for users to build the Beckhoff SSC Library with support for non-evaluation hardware.
-
[DTKEC-301] Test on AM243x EVM Hardware
Stack on AM243x EVM passed ETG conformance tool automated tests.
-
[DTKEC-732] Integrate documentation of the OBD and Process Data configuration in Doxygen
Extended documentation from ETG documents. See chapter EtherCAT SDK FAQ.
Bugfixes:
-
[DTKEC-742] Improve firmware load stability on AM243EVM and AM64EVM
- a former need call has been removed, which makes download of EtherCAT SDK more likely successful
-
[DTKEC-730] Build Warning still prevalent on the AM243x LP
Removed duplicate definitions from board config code.
-
[DTKEC-731] Solve issue of loading firmware to the core
Removed stale MPU configuration entry from sysconfig for AM64x-EVM.
Release Version 1.06.00
New Features:
Bugfixes:
-
[DTKEC-673] FreeRTOS debug support
- Fix linker files to make examples debuggable again
- Reduce memory usage of IP protection security algorithms
-
[DTKEC-675] FreeRTOS thread stacks
- Move thread stack variables to dedicated linker / memory section to avoid overwrite from stack manager
Release Version 1.05.02
Bugfixes:
-
[DTKEC-645] Version incorrectly displayed
- Incorrect version was displayed in the previous release.
Release Version 1.05.01
Bugfixes:
-
[DTKEC-631] Datasheet memory information missing
- Minor documentation corrections
Release Version 1.05.00
New Features:
-
[DTKEC-573] MCU+ SDK 8.01.00.35
- Update to MCU+ SDK 8.01.00.35
-
[DTKEC-342] Protection of intellectual property
- Add new chip-based license verification
Release Version 1.04.06
New Features:
-
[DTKEC-528] MCU+ SDK 8.01.00.26
- Updated to MCU+ SDK 8.01.00.26 to and Code Composer 11
Release Version 1.04.05
New Features:
-
[DTKEC-474] Documentation
- Update datasheet and add key performance parameter information
- Remove references to SDK API from CiA-402 example
- Fixed hyperlinks from Simple example documentation
-
[DTKEC-473] SysConfig AM243-EVM
Remove obsolete DDR4 RAM entry from MPU configuration on AM64-EVM and AM243-EVM
-
[DTKEC-472] Analyze library size differences
Use optimization for linkage Oz for all MCUs on FreeRTOS
Release Version 1.04.04
New Features:
-
[DTKEC-477] Automatic versioning
Add automatic global versioning to demo apps and remove some compile time warning.
-
[DTKEC-448] Documentation automation
Add size measurement to documentation
-
[DTKEC-403] Performance improvement
Add measurement callback functions and additional APIs which allow to directly access CoE objects to improve performance while accessing objects in control cycle (e.g. CiA 402).
-
[DTKEC-455] Remove next steps to build an example
Build an example description removed from documentation and replaced by Steps to Run the Example.
Release Version 1.04.03
New Features:
-
[DTKEC-372] Move "Supported Functionality" to the top level
The "Supported Functionality" section in the documentation has been moved from "General Information" to the top-level.
-
[DTKEC-402] Project name change
The project name has been changed from ethercat_linux to product_ethercat_slave.
-
[DTKEC-381] Reduce memory footprint
Stack is now compiled with THUMB mode. Additionally, the ESI parser has been moved to the application.
-
[DTKEC-394] Suppress linker warnings
The linker warnings have been corrected.
-
[DTKEC-395] OSAL_error 0x40000001 EC
Missing defines have been added to TI shipped example.projectspec(s) accordingly
-
[DTKEC-396] MCU+ SDK 8.01.00.10 Support
EtherCAT has been updated to support MCU+SDK 8.01.00.10.
-
[DTKEC-398] AM243x Heap size
The heap size for the AM243x applications has been reduced.
Release Version 1.04.02
New Features:
-
[DTKEC-343] MCU+ SDK 8.01.00.02 Support
MCU+ SDK 8.01.0.02 is now supported.
-
[DTKEC-243] Run and Error LED migrated TEST_LED_1 and TEST_LED_2
The run and error LEDs have been migrated to TEST_LED_1 and TEST_LED_2, respectively.
-
[DTKEC-167] Memory allocation reduction
The dynamically allocated memory footprint of the stack has been reduced. Additionally, the stack
memory access has been migrated from DDR to MSRAM.
Bug Fixes:
-
[DTKEC-348] Both ports not working with AM243x LP
Corrected issue with no communication on the second port.
-
[DTKEC-334] Update linker files to load apps only from MSRAM
The linker scripts were not fully adjusted to support MSRAM. This has been corrected.
-
[DTKEC-318] Repeating "Data Transfer failed with transfer status -2" Message
The "Data Transfer failed with transfer status -2" message that repeatedly displayed in the console output has been resolved.
Release Version 1.04.01
New Features:
-
[DTKEC-303] Create Project for AM243X EVM
Created new Code Composer Studio project for AM243X EVM and created documentation for the new platform.
Bug Fixes:
-
[DTKEC-317] Fix startup stability issue
Allocation of the stack size has been changed to the expected value. The larger size led to instabilities while booting up.
Release Version 1.04.00
New Features:
-
[DTKEC-256] MCU+ SDK 08.00.00.08 Support
EtherCAT has been updated to support MCU+ SDK 08.00.00.08.
-
[DTKEC-283] Create Project for AM24X
Created new Code Composer Studio project for AM243 and created documentation for the new platform.
Bug Fixes:
-
[DTKEC-250] Fix ESI file content for Simple, CTT and CIA402
Corrected inconsistencies between all ESI files.
-
[DTKEC-247] AM64x ESI file fix
Corrected access to PDO Mapping.
Release Version 1.03.01
New Features:
-
[DTKEC-237] AM64 Demo refactoring
Split of OS and MCU support files in DemoApps
Add conformance test tool Demo sources
Add CiA402 Demo sources
Release Version 1.03.00
New Features:
-
[DTKEC-162] CiA402 3 axes application example
Configuration of the CiA402 Object Dictionary and Process Data mapping described on ETG6010 Chapter 11 & 16.
ESI File (EtherCAT Device Description file) for the CiA402 example.
CiA402 state machine test. CiA402 is based on a state machine described in ETG6010 Chapter 5.
Bug Fixes:
-
[DTKEC-228] AM64 Startup problems corrected
Updated to support MCU plus 7.3.1.07.
Release Version 1.02.03
New Features:
-
[P2102-1] EtherCAT AM64 Porting to FreeRTOS
Support for FreeRTOS R5 on AM64 controller has been added. Tickets included: P2101-2->9; P2101-11->16; P2101-19->29
Release Version 1.02.00
New Features:
Release Version 1.01.01
New Features:
-
Abstraction Layer baseline adopted to migrate to SDK7 in next Release
Release Version 1.01.00
New Features: