Used to structures defining the Tamagawa interface, PRU slice and register offsets.
Data Fields | |
int32_t | channel |
uint16_t | rx_en_cnt |
struct tamagawa_xchg * | tamagawa_xchg |
void * | pruss_cfg |
int32_t | slice_value |
struct register_offsets | register_offset_val |
void * | pruss_iep |
uint64_t | cmp3 |
uint64_t | cmp0 |
int32_t tamagawa_priv::channel |
Holds the ID of the current channel being used
uint16_t tamagawa_priv::rx_en_cnt |
struct tamagawa_xchg* tamagawa_priv::tamagawa_xchg |
Structure defining Tamagawa interface
void* tamagawa_priv::pruss_cfg |
ICSS PRU config base address
int32_t tamagawa_priv::slice_value |
PRUx Slice being used
struct register_offsets tamagawa_priv::register_offset_val |
Register offset values based on PRUx slice selection
void* tamagawa_priv::pruss_iep |
ICSS IEP base address
uint64_t tamagawa_priv::cmp3 |
IEP CMP3 reg used in periodic trigger mode
uint64_t tamagawa_priv::cmp0 |
IEP CMP0 reg used in periodic trigger mode to reset IEP