AM243x Motor Control SDK  09.02.00
rx_frames_received Struct Reference

Detailed Description

Tamagawa Interface Received data.

Data Fields

uint32_t abs
 
uint32_t abm
 
uint8_t cf
 
uint8_t sf
 
uint8_t enid
 
uint8_t almc
 
uint8_t adf
 
uint8_t edf
 
uint8_t crc
 

Field Documentation

◆ abs

uint32_t rx_frames_received::abs

Data in one revolution

◆ abm

uint32_t rx_frames_received::abm

Multi-turn Data

◆ cf

uint8_t rx_frames_received::cf

Control Frame

◆ sf

uint8_t rx_frames_received::sf

Status Frame

◆ enid

uint8_t rx_frames_received::enid

Encoder ID

◆ almc

uint8_t rx_frames_received::almc

Encoder error

◆ adf

uint8_t rx_frames_received::adf

EEPROM address

◆ edf

uint8_t rx_frames_received::edf

EEPROM data

◆ crc

uint8_t rx_frames_received::crc

CRC