Data Fields | |
uint32_t | address |
uint32_t | data |
uint32_t | block |
uint8_t | has_block_address |
uint32_t | frequency |
uint64_t | cmp0 |
uint64_t | cmp3 |
uint64_t | cmp5 |
uint64_t | cmp6 |
uint32_t cmd_supplement::address |
uint32_t cmd_supplement::data |
uint32_t cmd_supplement::block |
uint8_t cmd_supplement::has_block_address |
uint32_t cmd_supplement::frequency |
uint64_t cmd_supplement::cmp0 |
uint64_t cmd_supplement::cmp3 |
uint64_t cmd_supplement::cmp5 |
uint64_t cmd_supplement::cmp6 |