Defines the Svgen Current object.
Data Fields | |
int16_t | minWidth |
The maximum width where a valid measurement cannot be taken. More... | |
SVGENCURRENT_IgnoreShunt_e | ignoreShunt |
Output of what shunt or shunts to ignore. More... | |
SVGENCURRENT_MeasureShunt_e | compMode |
Output phase compensation mode. More... | |
SVGENCURRENT_VmidShunt_e | Vmid |
The middle amplitude voltage among the three phase voltages. More... | |
float32_t | Vlimit |
The maximum output voltage duty that current can be sampled. More... | |
int16_t | Voffset |
The offset. More... | |
int16_t SVGENCURRENT_Obj::minWidth |
The maximum width where a valid measurement cannot be taken.
SVGENCURRENT_IgnoreShunt_e SVGENCURRENT_Obj::ignoreShunt |
Output of what shunt or shunts to ignore.
SVGENCURRENT_MeasureShunt_e SVGENCURRENT_Obj::compMode |
Output phase compensation mode.
SVGENCURRENT_VmidShunt_e SVGENCURRENT_Obj::Vmid |
The middle amplitude voltage among the three phase voltages.
float32_t SVGENCURRENT_Obj::Vlimit |
The maximum output voltage duty that current can be sampled.
int16_t SVGENCURRENT_Obj::Voffset |
The offset.