PRUICSS PWM Attributes.
PRUICSS PWM Attributes. It contains PRUICSS PWM Signal attributes which should be configured.
The application must access any member variables of this structure using PRUICSS_PWM_Handle.
Data Fields | |
uint32_t | dutyCycle |
uint32_t | fallEdgeDelay |
uint32_t | riseEdgeDelay |
uint8_t | outputCfgInitialState |
uint8_t | outputCfgActiveState |
uint8_t | outputCfgTripState |
uint8_t | enable |
uint8_t | iepInstance |
uint8_t | compareEvent |
uint32_t PRUICSS_PWM_Attrs::dutyCycle |
uint32_t PRUICSS_PWM_Attrs::fallEdgeDelay |
uint32_t PRUICSS_PWM_Attrs::riseEdgeDelay |
uint8_t PRUICSS_PWM_Attrs::outputCfgInitialState |
uint8_t PRUICSS_PWM_Attrs::outputCfgActiveState |
uint8_t PRUICSS_PWM_Attrs::outputCfgTripState |
uint8_t PRUICSS_PWM_Attrs::enable |
uint8_t PRUICSS_PWM_Attrs::iepInstance |
uint8_t PRUICSS_PWM_Attrs::compareEvent |