Data Fields | |
uint32_t | reserved1 |
uint32_t | loadAddr1 |
uint32_t | runAddr1 |
uint32_t | size1 |
uint32_t | reserved2 |
uint32_t | loadAddr2 |
uint32_t | runAddr2 |
uint32_t | size2 |
uint32_t HDSL_CopyTable::reserved1 |
uint32_t HDSL_CopyTable::loadAddr1 |
Load Address of Part 1 of firmware
uint32_t HDSL_CopyTable::runAddr1 |
Run Address of Part 1 of firmware
uint32_t HDSL_CopyTable::size1 |
Size of Part 1 of firmware
uint32_t HDSL_CopyTable::reserved2 |
uint32_t HDSL_CopyTable::loadAddr2 |
Load Address of Part 2 of firmware
uint32_t HDSL_CopyTable::runAddr2 |
Run Address of Part 2 of firmware
uint32_t HDSL_CopyTable::size2 |
Size of Part 2 of firmware