AM243x Motor Control SDK  09.02.00

Introduction

Contains Maximum torque per ampere (MTPA) functions implementation.

Go to the source code of this file.

Data Structures

struct  MTPA_Handle
 Defines the MTPA object. More...
 

Macros

#define MTPA_LUT_INDEX_LD_MAX   20
 Defines the maximum length of LUT for Ld. More...
 
#define MTPA_LUT_INDEX_LQ_MAX   20
 Defines the maximum length of LUT for Lq. More...
 
#define MTPA_LUT_DELTA_CURRENT_LD_A   0.5
 Defines the current delta of LUT for Ld, A. More...
 
#define MTPA_LUT_DELTA_CURRENT_LD_A   0.5
 Defines the current delta of LUT for Ld, A. More...
 

Functions

void MTPA_computeParameters (MTPA_Handle handle, const float32_t Ls_d_H, const float32_t Ls_q_H, const float32_t flux_Wb)
 Computes the motor constant for MTPA module. More...
 
MTPA_Handle MTPA_init (void *pMemory, const size_t numBytes)
 Initializes the maximum torque per ampere (MTPA) module. More...
 
static void MTPA_disable (MTPA_Handle handle)
 Disables the MTPA. More...
 
static void MTPA_enable (MTPA_Handle handle)
 Enables the MTPA. More...
 
static float32_tMTPA_getCurrentAnglePhase_rad_addr (MTPA_Handle handle)
 Gets the stator current phase angle memory address. More...
 
static float32_t MTPA_getCurrentAngle_rad (MTPA_Handle handle)
 Gets the stator current phase angle value (angleCurrent_rad) More...
 
static float32_t MTPA_getKconst (MTPA_Handle handle)
 Gets the motor constant of MTPA. More...
 
static float32_tMTPA_getIs_ref_A_addr (MTPA_Handle handle)
 Gets the stator current reference memory address. More...
 
static bool MTPA_getFlagEnable (MTPA_Handle handle)
 Gets the enable controller flag value from the controller. More...
 
static float32_t MTPA_getId_ref_A (MTPA_Handle handle)
 Gets the direct current reference value (Id_ref_A) More...
 
static float32_t MTPA_getIq_ref_A (MTPA_Handle handle)
 Gets the quadrature current reference value (Iq_ref_A) More...
 
static float32_t MTPA_getIs_ref_A (MTPA_Handle handle)
 Gets the stator current reference value (Is_ref_A) More...
 
static void MTPA_setFlagEnable (MTPA_Handle handle, const bool flagEnable)
 Sets the enable flag. More...
 
static void MTPA_setCurrentAngle_rad (MTPA_Handle handle, const float32_t angleCurrent_rad)
 Sets the stator current phase angle value. More...
 
static void MTPA_setId_ref_A (MTPA_Handle handle, const float32_t Id_ref_A)
 Sets the direct current (Id_ref) reference vector value. More...
 
static void MTPA_setIq_ref_A (MTPA_Handle handle, const float32_t Iq_ref_A)
 Sets the quadrature current (Iq_ref) reference value. More...
 
static void MTPA_setIs_ref_A (MTPA_Handle handle, const float32_t Is_ref_A)
 Sets the stator current reference value (Is_ref) More...
 
static float32_t MTPA_updateLs_d_withLUT (MTPA_Handle handle, const float32_t Is_A)
 Update the motor inductances. More...
 
static float32_t MTPA_updateLs_q_withLUT (MTPA_Handle handle, const float32_t Is_A)
 Update the motor inductances. More...
 
static void MTPA_computeCurrentReference (MTPA_Handle handle, const float32_t Is_ref_A)
 Compute the current reference of MTPA. More...
 
static float32_t MTPA_computeCurrentAngle (MTPA_Handle handle, const float32_t Is_ref_A)
 Compute the current angle of MTPA. More...
 

Variables

const float32_t MTPA_Ld_tableData_H [MTPA_LUT_INDEX_LD_MAX+1]
 Defines the Ld array. More...
 
const float32_t MTPA_Lq_tableData_H [MTPA_LUT_INDEX_LQ_MAX+1]
 Defines the Lq array. More...