Defines ZPK3 strcture that represents a third order transfer function of poles and zeros.
Go to the source code of this file.
Data Structures | |
struct | DCL_ZPK3 |
Defines the DCL_ZPK3 structure. More... | |
struct | DCL_ZPK3F64 |
Defines the 64bit ZPK3 structure. More... | |
Macros | |
#define | ZPK3_DEFAULTS |
Defines default values to initialize the DCL_ZPK3 structure. More... | |
#define | ZPK3F64_DEFAULTS |
Defines default values to initialize the DCL_ZPK3F64 structure. More... | |
Functions | |
_DCL_CODE_ACCESS bool | DCL_isStableZpk3 (DCL_ZPK3 *q) |
Determines stability of a ZPK3 representation by checking pole magnitude. More... | |
_DCL_CODE_ACCESS bool | DCL_isStableZpk3F64 (DCL_ZPK3 *q) |
Determines stability of a ZPK3F64 representation by checking pole magnitude. More... | |