Contains 64-bit PID controller with its related structures and functions.
|
#define | PIDF64_SPS_DEFAULTS { 1.0L, 0.0L, 0.0L, 1.0L, 1.0L, 0.0L, 1.0L, -1.0L } |
| Defines default values to initialize the DCL_PIDF64 shadow structure. More...
|
|
#define | PIDF64_DEFAULTS |
| Defines default values to initialize the DCL_PID64 active structure. More...
|
|
#define | PIDF64_INT_DEFAULTS |
| Macro for internal default values to initialize DCL_PIDF64 Example: DCL_PIDF64 pid_ctrl = { .Kp = 1.0L, .Ki = 0.0L, ... .Umin = -1.0L, PIDF64_INT_DEFAULTS };. More...
|
|
#define | DCL_initPIDF64() &(DCL_PIDF64)PIDF64_DEFAULTS |
| Initialize DCL_PIDF64 struct with default parameters Example: DCL_PIDF64* pid_ctrl = DCL_initPID();. More...
|
|
#define | DCL_initPIDF64asParam(kp, ki, kd, kr, _c1, _c2, umax, umin) |
| Initialize DCL_PIDF64 struct with input controller parameters Example: DCL_PIDF64* pid_ctrl = DCL_initPIDF64asParam(1.0L,0.0L,0.0L,1.0L,1.0L,0.0L,1.0L,-1.0L);. More...
|
|
#define | DCL_initPIDF64asSPS(pid_ptr, sps_ptr) |
| Initialize DCL_PIDF64 struct with sps parameters Example: DCL_PIDF64_SPS pid_sps = { .Kp = , .Ki = , ...}; //initial parameter DCL_PIDF64 pid_ctrl; DCL_initPIasSPS(&pid_ctrl,&pid_sps);. More...
|
|
|
_DCL_CODE_ACCESS void | DCL_resetPIDF64 (DCL_PIDF64 *pid) |
| Resets PID64 internal storage data with interrupt protection. More...
|
|
_DCL_CODE_ACCESS void | DCL_forceUpdatePIDF64 (DCL_PIDF64 *pid) |
| Loads PIDF64 tuning parameter from its SPS parameter without interrupt protection. More...
|
|
_DCL_CODE_ACCESS void | DCL_updatePIDF64NoCheck (DCL_PIDF64 *pid) |
| Updates PID parameter from its SPS parameter with interrupt protection. More...
|
|
_DCL_CODE_ACCESS bool | DCL_updatePIDF64 (DCL_PIDF64 *pid) |
| A conditional update based on the update flag. If the update status is set, the function will update PIDF64 parameter from its SPS parameter and clear the status flag on completion. More...
|
|
_DCL_CODE_ACCESS void | DCL_setPIDF64filterBW (DCL_PIDF64 *pid, float64_t fc) |
| Loads the derivative path filter shadow coefficients. More...
|
|
_DCL_CODE_ACCESS void | DCL_setActivePIDF64filterBW (DCL_PIDF64 *pid, float64_t fc, float64_t T) |
| Loads the PID64 derivative path filter active coefficients. More...
|
|
_DCL_CODE_ACCESS float64_t | DCL_getPIDF64filterBW (DCL_PIDF64 *pid) |
| Returns the active derivative path filter bandwidth in Hz. More...
|
|
_DCL_CODE_ACCESS void | DCL_loadSeriesPIDF64asZPK (DCL_PIDF64 *pid, DCL_ZPK3F64 *zpk) |
| Configures a series PID controller parameter in ZPK form. More...
|
|
_DCL_CODE_ACCESS void | DCL_loadParallelPIDF64asZPK (DCL_PIDF64 *pid, DCL_ZPK3 *zpk) |
| Configures a parallel PID controller in ZPK form. More...
|
|
_DCL_CRIT_ACCESS float64_t | DCL_runPIDF64Series (DCL_PIDF64 *pid, float64_t rk, float64_t yk, float64_t lk) |
| Executes an ideal form PID64 controller. More...
|
|
_DCL_CRIT_ACCESS float64_t | DCL_runPIDF64Parallel (DCL_PIDF64 *pid, float64_t rk, float64_t yk, float64_t lk) |
| Executes an parallel form PID64 controller. More...
|
|