Contains 32-bit non-linear PID controller with its related structures and functions.
|
_DCL_CODE_ACCESS void | DCL_resetNLPID (DCL_NLPID *pid) |
| Resets NLPID internal storage data with interrupt protection. More...
|
|
_DCL_CODE_ACCESS void | DCL_forceUpdateNLPID (DCL_NLPID *pid) |
| Loads NLPID tuning parameter from its SPS parameter without interrupt protection. More...
|
|
_DCL_CODE_ACCESS void | DCL_updateNLPIDNoCheck (DCL_NLPID *pid) |
| Loads PID tuning parameter from its SPS parameter with interrupt protection. More...
|
|
_DCL_CODE_ACCESS bool | DCL_updateNLPID (DCL_NLPID *pid) |
| A conditional update based on the update flag. If the update status is set, the function will update NLPID parameter from its SPS parameter and clear the status flag on completion. More...
|
|
_DCL_CODE_ACCESS void | DCL_setNLPIDfilterBW (DCL_NLPID *pid, float32_t fc) |
| Loads the shadow derivative LP filter coefficients. More...
|
|
_DCL_CODE_ACCESS void | DCL_setActiveNLPIDfilterBW (DCL_NLPID *pid, float32_t fc, float32_t T) |
| Loads the NLPID derivative path filter active coefficients. More...
|
|
_DCL_CODE_ACCESS float32_t | DCL_getNLPIDfilterBW (DCL_NLPID *pid) |
| Returns the derivative LP filter bandwidth in Hz. More...
|
|
_DCL_CODE_ACCESS float32_t | DCL_getNLPIDgamma (float32_t alpha, float32_t delta) |
| Returns the linearized region gain for specified (alpha,delta) More...
|
|
_DCL_CODE_ACCESS float32_t | DCL_getNLPIDdelta (float32_t alpha, float32_t gamma) |
| Returns the semi-width of the linear gain region for specified (alpha,gamma) More...
|
|
_DCL_CODE_ACCESS void | DCL_setNLPIDgamma (DCL_NLPID *pid) |
| Computes the linearized gains for each path Note: active coefficients not update DCL_updateNLPID() called. More...
|
|
_DCL_CODE_ACCESS void | DCL_setActiveNLPIDgamma (DCL_NLPID *pid) |
| Computes the linearized gains for each path and loads the parameters in the active NLPID structure. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runNLPIDParallel (DCL_NLPID *pid, float32_t rk, float32_t yk, float32_t lk) |
| Executes a parallel form non-linear PID controller. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runNLPIDSeries (DCL_NLPID *pid, float32_t rk, float32_t yk, float32_t lk) |
| Executes a series form non-linear PID controller. More...
|
|
_DCL_CRIT_ACCESS float32_t | DCL_runNLF (float32_t x, float32_t alpha, float32_t delta) |
| Executes a basic non-linear control function. More...
|
|