Contains abc to alpha/beta/0 transform implementation.
Go to the source code of this file.
Macros | |
#define | IEEE754_TYPES |
#define | ONE_OVER_THREE 0.33333333333333f |
#define | ONE_OVER_SQRT_THREE 0.57735026918963f |
Typedefs | |
typedef float | float32_t |
typedef double | float64_t |
Functions | |
static void | CLARKE_run_threeInput (const float32_t inIa, const float32_t inIb, const float32_t inIc, float32_t *pIalpha, float32_t *pIbeta) |
Runs the Clarke transform module for three inputs. More... | |
static void | CLARKE_run_twoInput (const float32_t inIa, const float32_t inIb, float32_t *pIalpha, float32_t *pIbeta) |
Runs the Clarke transform module for two inputs. More... | |