AM243x Motor Control SDK  09.01.00

Introduction

Contains 32-bit PID controller with its related structures and functions.

Go to the source code of this file.

Data Structures

struct  DCL_PID_SPS
 Defines DCL_PID shadow parameter set used for updating controller parameter. More...
 
struct  dcl_pid
 DCL_PID object for storing PID specific parameters. More...
 

Macros

#define PID_SPS_DEFAULTS   { 1.0f, 0.0f, 0.0f, 1.0f, 1.0f, 0.0f, 1.0f, -1.0f }
 Defines default values to initialize DCL_PID_SPS. More...
 
#define PID_DEFAULTS
 Defines default values to initialize the DCL_PID structure. More...
 
#define PID_INT_DEFAULTS
 Macro for internal default values to initialize DCL_PID Example: DCL_PID pid_ctrl = { .Kp = 1.0f, .Ki = 0.0f, ... .Umin = -1.0f, PID_INT_DEFAULTS };. More...
 
#define DCL_initPID()   &(DCL_PID)PID_DEFAULTS
 Initialize DCL_PID struct with default parameters Example: DCL_PID* pid_ctrl = DCL_initPID();. More...
 
#define DCL_initPIDasParam(kp, ki, kd, kr, _c1, _c2, umax, umin)
 Initialize DCL_PID struct with input controller parameters Example: DCL_PID* pid_ctrl = DCL_initPIDasParam(1.0f,0.0f,0.0f,1.0f,1.0f,0.0f,1.0f,-1.0f); Note: input parameter needs to be in the same order as listed in PID_SPS struct. More...
 
#define DCL_initPIDasSPS(pid_ptr, sps_ptr)
 Initialize DCL_PID struct with SPS parameters Example: DCL_PID_SPS pid_sps = { .Kp = , .Ki = , ...}; //initial parameter DCL_PID pid_ctrl; DCL_initPIasSPS(&pid_ctrl,&pid_sps); Note: The newly declared DCL_PID structure will use the SPS input parameter as its attribute for sps. More...
 

Typedefs

typedef _DCL_VOLATILE struct dcl_pid DCL_PID
 
typedef _DCL_VOLATILE struct dcl_pidPID_Handle
 

Functions

_DCL_CODE_ACCESS void DCL_resetPID (DCL_PID *pid)
 Resets PID internal storage data with interrupt protection. More...
 
_DCL_CODE_ACCESS void DCL_forceUpdatePID (DCL_PID *pid)
 Loads PID tuning parameter from its SPS parameter without interrupt protection. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION void DCL_updatePIDNoCheck (DCL_PID *pid)
 Loads PID tuning parameter from its SPS parameter with interrupt protection. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION bool DCL_updatePID (DCL_PID *pid)
 A conditional update based on the update flag. If the update status is set, the function will update PID parameter from its SPS parameter and clear the status flag on completion. Note: Use DCL_getUpdateStatus(pid) to set the update status. More...
 
_DCL_CODE_ACCESS void DCL_setPIDfilterBW (DCL_PID *pid, float32_t fc)
 Loads the derivative path filter shadow coefficients. Note: Sampling period pid->css->T are used in the calculation. New coefficients take effect when DCL_updatePID() is called. More...
 
_DCL_CODE_ACCESS void DCL_setActivePIDfilterBW (DCL_PID *pid, float32_t fc, float32_t T)
 Loads the PID derivative path filter active coefficients Note: Sampling period pid->css->T are used in the calculation. New coefficients take effect immediately. SPS & CSS contents are unaffected.
More...
 
_DCL_CODE_ACCESS float32_t DCL_getPIDfilterBW (DCL_PID *pid)
 Calculates the active derivative path filter bandwidth in Hz. Note: Sampling period pid->css->T are used in the calculation. More...
 
_DCL_CODE_ACCESS void DCL_loadSeriesPIDasZPK (DCL_PID *pid, DCL_ZPK3 *zpk)
 Configures a series PID controller parameter in ZPK form. Note: Sampling period pid->css->T are used in the calculation. Parameters take effect after call to DCL_updatePID(). Only z1, z2 & p2 considered, p1 = 0 assumed. More...
 
_DCL_CODE_ACCESS void DCL_loadParallelPIDasZPK (DCL_PID *pid, DCL_ZPK3 *zpk)
 Configures a parallel PID controller in ZPK form. Note: Sampling period pid->css->T are used in the calculation. Parameters take effect after call to DCL_updatePID(). Only z1, z2 & p2 considered, p1 = 0 assumed. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION float32_t DCL_runPIDSeries (DCL_PID *pid, float32_t rk, float32_t yk, float32_t lk)
 Executes an ideal form PID controller. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION float32_t DCL_runPIDParallel (DCL_PID *pid, float32_t rk, float32_t yk, float32_t lk)
 Executes a parallel form PID controller. More...