AM243x Motor Control SDK  09.01.00

Introduction

Top level header that contains all DCL common strctures and functions.

Go to the source code of this file.

Macros

#define _DCL_CODE_ACCESS   static inline
 Defines the scope of dcl functions (static inline/extern inline/none) More...
 
#define _DCL_CODE_SECTION   __attribute__((section("dclfuncs")))
 Defines dcl function section that users can specify in the linker file(.cmd) and to accelerate performance by mapping to faster memory Note: only DCL_run and DCL_update are included by default. More...
 
#define _DCL_VOLATILE
 Defines volatile for DCL strctures Flags can be defined in dcl.h or user files before including DCL lib. More...
 
#define DCL_setBreakPoint()
 Set a software breakpoint assembly instruction. More...
 
#define DCL_disableInts()   0
 Define enable and disable interrupt operations. More...
 
#define DCL_restoreInts(v)
 

Typedefs

typedef float float32_t
 Defines single,double precision data type. Note: Assumes ABI to be TI_EABI, does not support legacy TI_COFF. More...
 
typedef double float64_t
 
typedef uint32_t dcl_interrupt_t