BISS-C diagnostic application does the following:
This application is controlled with a terminal interface using a serial over USB connection between the PC host and the EVM. Please connect a USB cable between the PC and the EVM/LP. A serial terminal application (like teraterm/ hyperterminal/ minicom) is then run on the host. To configure, select the serial port corresponding to the port emulated over USB by the EVM. The host serial port should be configured to 115200 baud, no parity, 1 stop bit and no flow control.
The BISS-C receiver firmware running on ICSS0-PRU1 provides a defined interface. The BISS-C diagnostic application interacts with the BISS-C receiver firmware interface. It then presents the user with menu options to select Data ID code. The application collects the data entered by the user and configures the relevant interface. Then via the BISS-C receiver interface, the command is triggered. Once the command completion is indicated by the interface, the status of the transaction is checked. If the Status indicates success, the result is presented to the user.
Folder/Files | Description |
---|---|
${SDK_INSTALL_PATH}/examples/motor_control/bissc_diagnostic | |
bissc_diagnostic.c | BISS-C diagnostic application |
${SDK_INSTALL_PATH}/source/motor_control/position_sense/bissc | |
firmware/ | Folder containing BISS-C PRU firmware sources. |
driver/ | BISS-C diagnostic driver. |
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 freertos |
ICSSG | ICSSG0 |
PRU | PRU1 (single channel, multi channel using single PRU) |
PRU1, RTU-PRU1, TXPRU1 (multi channel using three PRUs - load share mode) | |
Toolchain | ti-arm-clang |
Board | am243x-lp (2 channel and 1 channel examples) |
Example folder | examples/motor_control/bissc_diagnostic |
Designator | ON/OFF | Description |
---|---|---|
J11 | OFF | VSENSE/ISENSE select |
J13 | OFF | VSENSE/ISENSE select |
J17 | Pin 1-2 Connected | SDFM Clock Feedback Select |
J18/J19 | J18 OFF & J19 ON | Axis 1: Encoder/Resolver Voltage Select |
J20/J21 | J20 ON & J21 OFF | Axis 2: Encoder/Resolver Voltage Select |
J22 | OFF | Axis 1: Manchester Encoding Select |
J23 | OFF | Axis 2: Manchester Encoding Select |
J24 | OFF | Axis 1: RS485/DSL MUX |
J25 | OFF | Axis 2: RS485/DSL MUX |
J26 | OFF | VSENSE/ISENSE Select |
J27 | ON | 3WIRE/SDFM MUX |
J28 | OFF | 3WIRE MUX |
Shown below is a sample output when the application is run:
# | Name | Description | Pass/fail Criteria |
---|---|---|---|
1 | Data readout (absolute position data) | In this command we will receive: Absolute rotor position value, errors, and warnings | CRC success with ABS, E, W and CRC values printed in the terminal. |
2 | Control Communication | In this command we will receive: Absolute rotor position value, errors, and warnings, along with the result of the control communication command. | CRC success with ABS, E, W and CRC values of position data along with the control communication result printed in the terminal. |