This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!
Copyright (C) 2021 Texas Instruments Incorporated - https://www.ti.com/
Declarations for all message structures to read and write SWREV and KEYREV
Request message to set swrev
This message can only be sent by the host that is tied to root of trust through the secure tisci_boardcfg extended otp extension
hdr | Standard TISCI header |
identifier | One of the entries from enum tisci_otp_revision_identifier |
value | Revision value (integer) to be bit encoded, and programmed |
Data Fields | |
struct tisci_header | hdr |
uint8_t | identifier |
uint32_t | value |
struct tisci_header tisci_msg_set_swrev_req::hdr |
uint8_t tisci_msg_set_swrev_req::identifier |
uint32_t tisci_msg_set_swrev_req::value |