Structure representing the cb_socket_lldcfg_update instance.
Data Fields | |
const char * | dev |
uint16_t | proto |
uint16_t | vlanid |
uint32_t | nTxPkts |
uint32_t | nRxPkts |
uint32_t | pktSize |
int | dmaTxChId |
int | dmaRxChId |
bool | unusedDma |
const char* cb_socket_lldcfg_update_t::dev |
Device name to match the expected socket.
uint16_t cb_socket_lldcfg_update_t::proto |
Protocol or ethernet type in the ethernet frame header to match the expected socket.
uint16_t cb_socket_lldcfg_update_t::vlanid |
VLAN ID to match the expected socket.
uint32_t cb_socket_lldcfg_update_t::nTxPkts |
Number of buffers allocated for transmit packets Positive value will be updated to LLDEnetCfg_t.
uint32_t cb_socket_lldcfg_update_t::nRxPkts |
Number of buffers allocated for receive packets Positive value will be updated to LLDEnetCfg_t.
uint32_t cb_socket_lldcfg_update_t::pktSize |
Transmit and receive maximum packet size. Positive value will be updated to LLDEnetCfg_t.
int cb_socket_lldcfg_update_t::dmaTxChId |
DMA transmit channel ID. 0 or positive value will be updated to LLDEnetCfg_t
int cb_socket_lldcfg_update_t::dmaRxChId |
DMA receive channel ID. 0 or positive value will be updated to LLDEnetCfg_t
bool cb_socket_lldcfg_update_t::unusedDma |
true: won't use DMA, false: use DMA