Data Fields | |
HwiP_Object | interruptObject |
uint32_t | pruIntNum |
uint32_t | coreIntNum |
uint32_t | socEvId |
uint32_t | intPrio |
void * | args |
void * | isrFnPtr |
void * | callBackPtr |
HwiP_Object PN_IntAttrs::interruptObject |
uint32_t PN_IntAttrs::pruIntNum |
PRUICSS Interrupt number
uint32_t PN_IntAttrs::coreIntNum |
Core Interrupt number
uint32_t PN_IntAttrs::socEvId |
SoC event ID
uint32_t PN_IntAttrs::intPrio |
HWI priority
void* PN_IntAttrs::args |
HWI args
void* PN_IntAttrs::isrFnPtr |
Interrupt routine
void* PN_IntAttrs::callBackPtr |
Callback to the stack within the ISR