ICSS_EMAC Parameters.
ICSS_EMAC Parameters are used to with the ICSS_EMAC_open() call. Default values for these parameters are set using ICSS_EMAC_Params_init().
[MANDATORY] is present in the description for members which are mandatory.
Data Fields | |
PRUICSS_Handle | pruicssHandle |
const PRUICSS_IntcInitData * | pruicssIntcInitData |
ICSS_EMAC_FwStaticMmap * | fwStaticMMap |
ICSS_EMAC_FwDynamicMmap * | fwDynamicMMap |
ICSS_EMAC_FwVlanFilterParams * | fwVlanFilterParams |
ICSS_EMAC_FwMulticastFilterParams * | fwMulticastFilterParams |
ICSS_EMAC_CallBackObject | callBackObject |
ETHPHY_Handle | ethphyHandle [ICSS_EMAC_MAX_PORTS_PER_INSTANCE] |
uint8_t | macId [6] |
PRUICSS_Handle ICSS_EMAC_Params::pruicssHandle |
[MANDATORY] PRUICSS Handle for which the ICSS-EMAC driver will be based on
const PRUICSS_IntcInitData* ICSS_EMAC_Params::pruicssIntcInitData |
[MANDATORY] PRUICSS INTC mapping structure pointer needed for PRUICSS_intcInit call
ICSS_EMAC_FwStaticMmap* ICSS_EMAC_Params::fwStaticMMap |
[MANDATORY] Static Firmware Memory Map offsets
ICSS_EMAC_FwDynamicMmap* ICSS_EMAC_Params::fwDynamicMMap |
[MANDATORY] Dynamic Firmware Memory Map offsets
ICSS_EMAC_FwVlanFilterParams* ICSS_EMAC_Params::fwVlanFilterParams |
VLAN filtering related Firmware Memory Map offsets. Should be passed if IOCTL commands for VLAN filtering are going to be used
ICSS_EMAC_FwMulticastFilterParams* ICSS_EMAC_Params::fwMulticastFilterParams |
Multicast filtering related Firmware Memory Map offsets. Should be passed if IOCTL commands for Multicast filtering are going to be used
ICSS_EMAC_CallBackObject ICSS_EMAC_Params::callBackObject |
Callback functions for difference scenarios like link change, Rx for NRT/RT, Tx and Learning exception
ETHPHY_Handle ICSS_EMAC_Params::ethphyHandle[ICSS_EMAC_MAX_PORTS_PER_INSTANCE] |
[MANDATORY] Ethernet PHY Handle. For mac mode, ethphyHandle[0] is used. For switch mode, ethphyHandle[0] and ethphyHandle[1] are used.
uint8_t ICSS_EMAC_Params::macId[6] |
[MANDATORY] MacId to be used for the interface