Functions | |
void | PrpFrameFill (hsrPrpHandle *hsrPrphandle, RED_FRAME *pRedFrame, const uint8_t *pFrame, int32_t frameSize) |
void | PrpFrameUpdateLanId (RED_FRAME *pPrpFrame, uint16_t pathId) |
RED_FRAME * | PrpSupFrameAllocate (hsrPrpHandle *hsrPrphandle) |
Allocates a RED_FRAME that holds PRP Supervision frame. More... | |
void | PrpSupFrameUpdateSrcAdd (RED_FRAME *pRedFrame, uint8_t *srcAdd) |
Updates Source Address of a PRP Supervision frame. More... | |
void | PrpSupFrameUpdateLanId (RED_FRAME *pRedFrame, uint16_t lanId) |
Updates LAN ID of a PRP Supervision frame. More... | |
void | PrpSupFrameUpdateSeqNr (hsrPrpHandle *hsrPrphandle, RED_FRAME *pRedFrame) |
void | PrpSupFrameUpdateTlv (RED_FRAME *pRedFrame, uint8_t type) |
void | PrpSupFrameIncrementSeqNr (hsrPrpHandle *hsrPrphandle) |
void PrpFrameFill | ( | hsrPrpHandle * | hsrPrphandle, |
RED_FRAME * | pRedFrame, | ||
const uint8_t * | pFrame, | ||
int32_t | frameSize | ||
) |
void PrpFrameUpdateLanId | ( | RED_FRAME * | pPrpFrame, |
uint16_t | pathId | ||
) |
RED_FRAME* PrpSupFrameAllocate | ( | hsrPrpHandle * | hsrPrphandle | ) |
void PrpSupFrameUpdateSrcAdd | ( | RED_FRAME * | pRedFrame, |
uint8_t * | srcAdd | ||
) |
Updates Source Address of a PRP Supervision frame.
pRedFrame | pointer to a RED_FRAME |
srcAdd | pointer to a new source address value |
void PrpSupFrameUpdateLanId | ( | RED_FRAME * | pRedFrame, |
uint16_t | lanId | ||
) |
Updates LAN ID of a PRP Supervision frame.
pRedFrame | pointer to a RED_FRAME |
lanId | LAN ID value |
void PrpSupFrameUpdateSeqNr | ( | hsrPrpHandle * | hsrPrphandle, |
RED_FRAME * | pRedFrame | ||
) |
void PrpSupFrameUpdateTlv | ( | RED_FRAME * | pRedFrame, |
uint8_t | type | ||
) |
void PrpSupFrameIncrementSeqNr | ( | hsrPrpHandle * | hsrPrphandle | ) |