Functions | |
int32_t | PN_setWatchDogTimer (PN_Handle pnHandle, int32_t timerPeriod) |
API to configure the ICSS watchdog expiry duration. More... | |
int32_t PN_setWatchDogTimer | ( | PN_Handle | pnHandle, |
int32_t | timerPeriod | ||
) |
API to configure the ICSS watchdog expiry duration.
pnHandle | Profinet Handle | |
[in] | timerPeriod | Time duration (in milliseconds) after which watchdog expires if not tapped in-between. Valid range is from 2 ms to 6553 ms |
0 | on success |