Tamagawa EEPROM Interface.
Data Fields | |
volatile uint32_t | cmd |
volatile uint32_t | adf |
volatile uint32_t | edf |
volatile uint32_t | crc |
volatile uint32_t | word0 |
volatile uint32_t | word1 |
volatile uint32_t | word2 |
uint64_t | eeprom_tx_data |
volatile uint32_t tamagawa_eeprom_interface::cmd |
holds the value of command id for EEPROM commands
volatile uint32_t tamagawa_eeprom_interface::adf |
holds the value of ADF for EEPROM commands
volatile uint32_t tamagawa_eeprom_interface::edf |
holds the value of EDF for EEPROM Write command
volatile uint32_t tamagawa_eeprom_interface::crc |
holds the value of CRC for EEPROM commands
volatile uint32_t tamagawa_eeprom_interface::word0 |
used for CRC calculation
volatile uint32_t tamagawa_eeprom_interface::word1 |
used for CRC calculation
volatile uint32_t tamagawa_eeprom_interface::word2 |
used for CRC calculation
uint64_t tamagawa_eeprom_interface::eeprom_tx_data |
used to store the bits for tx in eeprom read/write