AM243x Motor Control SDK  09.00.00
dcl_df11.h File Reference

Introduction

Contains direct form 1 1st order DF11 compensator with its related structures and functions.

Go to the source code of this file.

Data Structures

struct  DCL_DF11_SPS
 Defines DCL_DF11 shadow parameter set used for updating compensator parameter. More...
 
struct  dcl_df11
 DCL_DF11 object for storing df11 specific parameters. More...
 

Macros

#define DF11_SPS_DEFAULTS   { 0.5f, 0.5f, 1.0f }
 
#define DF11_DEFAULTS
 Defines default values to initialize DCL_DF11. More...
 
#define DF11_INT_DEFAULTS   .d1=0.0f, .d2=0.0f, .sps=&(DCL_DF11_SPS)DF11_SPS_DEFAULTS, .css=&(DCL_CSS)DCL_CSS_DEFAULTS
 Macro for internal default values to initialize DCL_DF11 Example: DCL_DF11 df11_ctrl = { .b0 = 0.5f, .b1 = 0.5f, .a1 = 1.0f, DF11_INT_DEFAULTS };. More...
 
#define DCL_initDF11()   &(DCL_DF11)DF11_DEFAULTS
 Initialize DCL_DF11 struct with default parameters Example: DCL_DF11* df11_ctrl = DCL_initDF11();. More...
 
#define DCL_initDF11asParam(_b0, _b1, _a1)
 Initialize DCL_DF11 struct with input compensator parameters Example: DCL_DF11* DF11_ctrl = DCL_initDF11asParam(0.5f,0.5f,1.0f); Note: input parameter needs to be in the same order as listed in DF11_SPS struct. More...
 
#define DCL_initDF11asSPS(df_ptr, sps_ptr)
 Initialize DCL_DF11 struct with sps parameters Example: DCL_DF11_SPS df_sps = { .b0 = , .b1 = , ...}; //initial parameter DCL_DF11 df_ctrl; DCL_initDF11asSPS(&df_ctrl,&df_sps);. More...
 

Typedefs

typedef _DCL_VOLATILE struct dcl_df11 DCL_DF11
 
typedef _DCL_VOLATILE struct dcl_df11DF11_Handle
 

Functions

_DCL_CODE_ACCESS void DCL_resetDF11 (DCL_DF11 *df)
 Resets DF11 internal storage data with interrupt protection. More...
 
_DCL_CODE_ACCESS void DCL_fupdateDF11 (DCL_DF11 *df)
 Loads DF11 tuning parameter from its SPS parameter. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION bool DCL_updateDF11 (DCL_DF11 *df)
 Updates DF11 parameter from its SPS parameter with interrupt protection. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION bool DCL_pendingUpdateDF11 (DCL_DF11 *df)
 A conditional update based on the pending-for-update flag. If the pending status is set, the function will update DF11 parameter from its SPS parameter and clear the status flag on completion. Note: Use DCL_setPendingStatus(df) to set the pending status. More...
 
_DCL_CODE_ACCESS void DCL_updateDF11SPS (DCL_DF11 *df)
 Update SPS parameter with active param, userful when needing to update only few active param from SPS and keep rest the same
More...
 
_DCL_CODE_ACCESS bool DCL_isStableDF11 (DCL_DF11 *df)
 Determines stability of the shadow DF11 compensator. More...
 
_DCL_CODE_ACCESS void DCL_loadDF11asZPK (DCL_DF11 *df, DCL_ZPK3 *zpk)
 Loads the DF11 shadow coefficients from a ZPK3 description Note: Sampling period df->css->t_sec are used in the calculation. New settings take effect after DCL_updateDF11(). Only real z1 & p1 considered, all other roots ignored. More...
 
_DCL_CODE_ACCESS void DCL_loadDF11asPI (DCL_DF11 *df, float32_t Kp, float32_t Ki)
 Loads compensator coefficients to emulate series form PI Note: Sampling period df->css->t_sec are used in the calculation. New settings take effect after DCL_updateDF11(). More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION float32_t DCL_runDF11 (DCL_DF11 *df, float32_t ek)
 Executes a 1st order Direct Form 1 controller. More...