AM64x INDUSTRIAL COMMUNICATIONS SDK  2026.00.00

Detailed Description

LRE Interface Statistics.

Data Fields

uint32_t cntUniqueA
 
uint32_t cntUniqueB
 
uint32_t cntDuplicateA
 
uint32_t cntDuplicateB
 
uint32_t cntMultiA
 
uint32_t cntMultiB
 
uint32_t cntRxA
 
uint32_t cntRxB
 
uint32_t cntTxA
 
uint32_t cntTxB
 
uint32_t cntOwnRxA
 
uint32_t cntOwnRxB
 
uint32_t cntErrWrongLanA
 
uint32_t cntErrWrongLanB
 
uint32_t cntErrorsA
 
uint32_t cntErrorsB
 
uint32_t cntUniqueC
 
uint32_t cntDuplicateC
 
uint32_t cntMultiC
 
uint32_t cntRxC
 
uint32_t cntTxC
 
uint32_t cntErrWrongLanC
 
uint32_t cntErrorsC
 
uint32_t cntNodes
 
uint32_t cntProxyNodes
 

Field Documentation

◆ cntUniqueA

uint32_t lreStatistics::cntUniqueA

Number of entries in the duplicate detection mechanism on port A for which no duplicate was received

◆ cntUniqueB

uint32_t lreStatistics::cntUniqueB

Number of entries in the duplicate detection mechanism on port B for which no duplicate was received

◆ cntDuplicateA

uint32_t lreStatistics::cntDuplicateA

Number of entries in the duplicate detection mechanism on port A for which one single duplicate was received

◆ cntDuplicateB

uint32_t lreStatistics::cntDuplicateB

Number of entries in the duplicate detection mechanism on port B for which one single duplicate was received

◆ cntMultiA

uint32_t lreStatistics::cntMultiA

Number of entries in the duplicate detection mechanism on port A for which more than one duplicate was received

◆ cntMultiB

uint32_t lreStatistics::cntMultiB

Number of entries in the duplicate detection mechanism on port B for which more than one duplicate was received

◆ cntRxA

uint32_t lreStatistics::cntRxA

Number of frames received on the LRE port A

◆ cntRxB

uint32_t lreStatistics::cntRxB

Number of frames received on the LRE port B

◆ cntTxA

uint32_t lreStatistics::cntTxA

Number of frames sent over port A that are HSR tagged

◆ cntTxB

uint32_t lreStatistics::cntTxB

Number of frames sent over port B that are HSR tagged

◆ cntOwnRxA

uint32_t lreStatistics::cntOwnRxA

Number of HSR tagged frames received on port A that originated from this device

◆ cntOwnRxB

uint32_t lreStatistics::cntOwnRxB

Number of HSR tagged frames received on port B that originated from this device

◆ cntErrWrongLanA

uint32_t lreStatistics::cntErrWrongLanA

Number of frames with the wrong LAN identifier received on the LRE port A

◆ cntErrWrongLanB

uint32_t lreStatistics::cntErrWrongLanB

Number of frames with the wrong LAN identifier received on the LRE port B

◆ cntErrorsA

uint32_t lreStatistics::cntErrorsA

Number of frames with errors received on the LRE port A

◆ cntErrorsB

uint32_t lreStatistics::cntErrorsB

Number of frames with errors received on the LRE port B

◆ cntUniqueC

uint32_t lreStatistics::cntUniqueC

Number of entries in the duplicate detection mechanism on application interface for which no duplicate was received

◆ cntDuplicateC

uint32_t lreStatistics::cntDuplicateC

Number of entries in the duplicate detection mechanism on the application interface of the DAN for which one single duplicate was received

◆ cntMultiC

uint32_t lreStatistics::cntMultiC

Number of entries in the duplicate detection mechanism on the application interface of the DAN for which more than one duplicate was received

◆ cntRxC

uint32_t lreStatistics::cntRxC

Number of frames received from the application interface of the DAN

◆ cntTxC

uint32_t lreStatistics::cntTxC

Number of frames sent towards the application interface of the DAN

◆ cntErrWrongLanC

uint32_t lreStatistics::cntErrWrongLanC

Number of frames with the wrong LAN identifier received on the interlink

◆ cntErrorsC

uint32_t lreStatistics::cntErrorsC

Number of frames with errors received on the application interface of the DAN

◆ cntNodes

uint32_t lreStatistics::cntNodes

Number of entries in the node table

◆ cntProxyNodes

uint32_t lreStatistics::cntProxyNodes

Number of entries in the proxy table