DLR parent structure through which all other structures can be accessed.
Data Fields | |
| superConfig | supConfig |
| activeSuperAddr | addr |
| dlrStateMachineVar | SMVariables |
| uint32_t | dlrCapabilities |
| uint8_t | activeSuperPred |
| HwiP_Object | port0IntObject |
| HwiP_Object | port1IntObject |
| HwiP_Object | beaconTimeoutIntP0Object |
| HwiP_Object | beaconTimeoutIntP1Object |
| HwiP_Object | announceSuppressionTimeoutIntObject |
| uint32_t | port0IntNum |
| uint32_t | port1IntNum |
| uint32_t | beaconTimeoutIntNum_P0 |
| uint32_t | beaconTimeoutIntNum_P1 |
| uint8_t | isSwitchOverPeriodActive |
| uint8_t | configChangeSuppressionActive |
| lastActiveNode | activeNode [2] |
| uint16_t | numRingFaultsSincePowerUp |
| uint16_t | ringParticipantsCount |
| protocolParticipants | ringNodes [DLR_MAX_NODES_SUPPORTED] |
| uint8_t | isSupervisorSupported |
| superConfig dlrStruct::supConfig |
Supervisor config. Attribute ID 4
| activeSuperAddr dlrStruct::addr |
Supervisor address. Attribute ID 10
| dlrStateMachineVar dlrStruct::SMVariables |
State Machine variables. Attributes 1 through 3
| uint32_t dlrStruct::dlrCapabilities |
DLR Capabilities, flag The Map is as follows 0 : Announce Based Ring Node 1 : Beacon based Ring Node 2-4 : Reserved 5 : Supervisor capable 6 : Redundant capable 7 : Flush Table frame capable 8-31 : Reserved DLR Capabilities of the device. Attribute ID 12
| uint8_t dlrStruct::activeSuperPred |
Active Supervisor precedence. Attribute ID 11
| HwiP_Object dlrStruct::port0IntObject |
| HwiP_Object dlrStruct::port1IntObject |
| HwiP_Object dlrStruct::beaconTimeoutIntP0Object |
| HwiP_Object dlrStruct::beaconTimeoutIntP1Object |
| HwiP_Object dlrStruct::announceSuppressionTimeoutIntObject |
| uint32_t dlrStruct::port0IntNum |
DLR Port 0 Interrupt number for ARM
| uint32_t dlrStruct::port1IntNum |
DLR Port 1 Interrupt number for ARM
| uint32_t dlrStruct::beaconTimeoutIntNum_P0 |
DLR interrupt for beacon timeout for Port 0
| uint32_t dlrStruct::beaconTimeoutIntNum_P1 |
DLR interrupt for beacon timeout for Port 1
| uint8_t dlrStruct::isSwitchOverPeriodActive |
Flag to indicate if switch over period is active
| uint8_t dlrStruct::configChangeSuppressionActive |
Flag to indicate that the active ring supervisor parameters have changed and its waiting for the 2x beacon timeout before restarting beacon transmission
| lastActiveNode dlrStruct::activeNode[2] |
Attribute ID's 6 and 7
| uint16_t dlrStruct::numRingFaultsSincePowerUp |
Number of Ring Faults since power up. Attribute ID 5
| uint16_t dlrStruct::ringParticipantsCount |
Number of ring participants. Attribute ID 8
| protocolParticipants dlrStruct::ringNodes[DLR_MAX_NODES_SUPPORTED] |
pointer to array of structures. Attribute ID 9
| uint8_t dlrStruct::isSupervisorSupported |
variable to track if supervisor is supported - need to be set from the application