IO-Link Master Firmware Hardware Abstraction Layer (FWHAL) API.
This header provides the public API for the IO-Link Master FWHAL module, which abstracts the PRU-ICSS firmware for IO-Link communication.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Go to the source code of this file.
Data Structures | |
| struct | IOLFW_PortInst_t |
| IO-Link port instance data. More... | |
| struct | IOLFW_Inst_t |
| IOLFW instance handle. More... | |
| struct | IOLFW_GpioConfig_t |
| GPIO pin configuration. More... | |
| struct | IOLFW_GpioPruConfig_t |
| GPIO configuration with PRU pin mapping. More... | |
| struct | IOLFW_GpioEnConfig_t |
| GPIO enable configuration with PRU direct access. More... | |
| struct | IOLFW_PortConfig_t |
| IO-Link port hardware configuration. More... | |
| struct | IOLFW_Config_t |
| IOLFW initialization configuration. More... | |
| struct | IOLFW_PlCallbacks_t |
| Physical Layer (PL) callbacks. More... | |
| struct | IOLFW_SpCallbacks_t |
| Stack Porting Layer (SP) callbacks. More... | |
Typedefs | |
| typedef struct IOLFW_PruMem | IOLFW_PruMem_t |
| typedef struct IOLFW_PruMemTimer | IOLFW_PruMemTimer_t |
| typedef void(* | IOLFW_cbSetMode_t) (IOLFW_Inst_t *pFwInstance, uint8_t portNum, IOLFW_ePortMode_t mode) |
| Port mode change callback. More... | |
| typedef const IOLFW_PortConfig_t *(* | IOLFW_cbGetPortCfg_t) (IOLFW_Inst_t *pFwInstance, uint8_t portNum) |
| Get port configuration callback. More... | |
| typedef void(* | IOLFW_cbRxErrEvent_t) (IOLFW_Inst_t *pFwInstance, uint8_t port, IOLFW_eRxErrorEvents_t rxErr) |
| RX error event callback. More... | |
| typedef void(* | IOLFW_cbTransferInd_t) (IOLFW_Inst_t *pFwInstance, uint8_t port, uint8_t dataLen, IOLFW_eTransferStatus_t eTrStatus) |
| Transfer indication callback. More... | |
| typedef void(* | IOLFW_cbStartupCmpl_t) (IOLFW_Inst_t *pFwInstance, uint8_t port, IOLFW_eStartupStatus_t eStrStatus) |
| Startup/wake-up completion callback. More... | |
| typedef IOLFW_Inst_t *(* | IOLFW_cbGetInstCont_t) (uint8_t inst_p) |
| Get instance container callback. More... | |
Enumerations | |
| enum | IOLFW_ePortMode_t { IOLFW_ePortMode_SioInactive = 0, IOLFW_ePortMode_Sdci, IOLFW_ePortMode_SioDI, IOLFW_ePortMode_SioDO, IOLFW_ePortMode_Force32Bit = 0x7fffffff } |
| IO-Link port operating mode. More... | |
| enum | IOLFW_eInstanceState_t { IOLFW_eInstanceState_NotInitialized = 0, IOLFW_eInstanceState_Init, IOLFW_eInstanceState_Running } |
| IOLFW instance state. More... | |
| enum | IOLFW_eBaudrate_t { IOLFW_eBaudrate_Auto = 0, IOLFW_eBaudrate_Com1, IOLFW_eBaudrate_Com2, IOLFW_eBaudrate_Com3 } |
| IO-Link transmission rate (baud rate) More... | |
| enum | IOLFW_eRxErrorEvents_t { IOLFW_eRxErrorEvents_Rxol = 0 } |
| RX error event types. More... | |
| enum | IOLFW_eTransferStatus_t { IOLFW_eTransferStatus_Ok = 0, IOLFW_eTransferStatus_ParityError, IOLFW_eTransferStatus_FramingError, IOLFW_eTransferStatus_Overrun } |
| Data transfer status codes. More... | |
| enum | IOLFW_eStartupStatus_t { IOLFW_eStartupStatus_Ok = 0, IOLFW_eStartupStatus_NoResponse } |
| Port startup/wake-up status codes. More... | |
Functions | |
Callback Registration Functions | |
| void | IOLFW_registerSetModeCallback (IOLFW_cbSetMode_t pCallback) |
| Register port mode change callback. More... | |
| void | IOLFW_registerGetPortCfgCallback (IOLFW_cbGetPortCfg_t pCallback) |
| Register port configuration callback. More... | |
| void | IOLFW_registerRxErrEventCallback (IOLFW_cbRxErrEvent_t pCallback) |
| Register RX error event callback. More... | |
| void | IOLFW_registerTransferIndCallback (IOLFW_cbTransferInd_t pCallback) |
| Register transfer indication callback. More... | |
| void | IOLFW_registerStartupCmplCallback (IOLFW_cbStartupCmpl_t pCallback) |
| Register startup completion callback. More... | |
Initialization Functions | |
| int32_t | IOLFW_init (IOLFW_Inst_t **pFwInstance, IOLFW_Config_t *pConfig) |
| Initialize IOLFW instance. More... | |
| int32_t | IOLFW_deInit (IOLFW_Inst_t *pFwInstance) |
| De-initialize IOLFW instance. More... | |
Port Operations | |
| int32_t | IOLFW_setPortMode (IOLFW_Inst_t *pFwInstance, uint8_t port, IOLFW_ePortMode_t eTargetMode) |
| Set port operating mode. More... | |
| IOLFW_eBaudrate_t | IOLFW_getBaudRate (IOLFW_Inst_t *pFwInstance, uint8_t port) |
| Get current baud rate of port. More... | |
| int32_t | IOLFW_wakeUp (IOLFW_Inst_t *pFwInstance, uint8_t port) |
| Initiate IO-Link wake-up sequence. More... | |
| int32_t | IOLFW_transferPrepare (IOLFW_Inst_t *pFwInstance, uint8_t port, uint8_t *pData, uint8_t dataLength, uint8_t *pResponseData, uint8_t responseLength) |
| Prepare data transfer. More... | |
Cycle Timer Functions | |
| int32_t | IOLFW_setMaxRespTime (IOLFW_Inst_t *pFwInstance, uint8_t port, uint8_t taRespTime) |
| Set maximum response time. More... | |
| int32_t | IOLFW_resetCycleTime (IOLFW_Inst_t *pFwInstance, uint8_t port) |
| Reset cycle timer counter. More... | |
| int32_t | IOLFW_setCycleTime (IOLFW_Inst_t *pFwInstance, uint8_t port, uint32_t timeUs) |
| Set cycle time. More... | |
| int32_t | IOLFW_enableCycleTimer (IOLFW_Inst_t *pFwInstance, uint8_t port, bool enable) |
| Enable or disable cycle timer. More... | |
| int32_t | IOLFW_configCycleTime (IOLFW_Inst_t *pFwInstance, uint8_t port, uint32_t timeUs) |
| Configure and enable cycle time. More... | |