|
| int32_t | PN_initDrv (PN_Handle pnHandle) |
| | Initializes the Profinet Driver. More...
|
| |
| void | PN_getFirmwareVersion (uint32_t *version_major, uint32_t *version_minor, uint32_t *version_build, uint32_t *version_release_type) |
| | Get the details on version of firmware. More...
|
| |
| void | PN_getFirmwareReleaseInfoAndFeatures (uint32_t *firmware_release_1, uint32_t *firmware_release_2, uint32_t *firmware_feature_mask) |
| | Get the details on release information and features of firmware. More...
|
| |
| int32_t | PN_setDcpFilterStationName (PRUICSS_HwAttrs const *pruicssHwAttrs, const uint8_t *dcpNameOfStation, uint8_t lengthOfStationName) |
| | API to configure the station name and length of station name of device for filtering DCP Identify requests. More...
|
| |
| int32_t | PN_MRP_setPortState (PN_Handle pnHandle, uint8_t portNumber, uint8_t pState) |
| | API to set the MRP state for a port. More...
|
| |
| int32_t | PN_MRP_getPortState (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t portNumber, uint8_t *pState) |
| | Returns the MRP state of a port. More...
|
| |
| int32_t | PN_mapPhaseToProfile (PRUICSS_HwAttrs const *pruicssHwAttrs, int32_t portNumber, int32_t phaseNumber, int32_t profileNumberRx, int32_t profileNumberTx) |
| | API to map a Phase to start of green Profile. More...
|
| |
| int32_t | PN_setMaxLineRxDelay (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t portNumber, int32_t maxLineRxDelayValue) |
| | API to configure the maximum line receive delay. More...
|
| |
| int32_t | PN_setMaxBridgeDelay (PRUICSS_HwAttrs const *pruicssHwAttrs, int32_t maxBridgeDelayValue) |
| | API to configure the maximum bridge delay. This value comes from the GSD file. More...
|
| |
| int32_t | PN_setYellowPeriod (PRUICSS_HwAttrs const *pruicssHwAttrs, int32_t yellowPeriodTime) |
| | API to configure the yellow period. More...
|
| |
| int32_t | PN_setProfile (PRUICSS_HwAttrs const *pruicssHwAttrs, int32_t portNumber, int32_t profileNumber, int32_t rxSoGValue, int32_t txSoGValue) |
| | API to configure a Profile. In a profile the start of green time in a cycle for Receive (Rx) and Transmit (Tx) is set for a port. More...
|
| |
| void | PN_setCompensationValue (PRUICSS_HwAttrs const *pruicssHwAttrs, uint16_t compensationValue) |
| | API to configure the compensation value which is used while computing the forward FSO for a RTC3 frame which has to be forwarded. More...
|
| |
| int32_t | PN_setRedGuard (PRUICSS_HwAttrs const *pruicssHwAttrs, uint16_t validLowerFrameId, uint16_t validUpperFrameId) |
| | API to set the Red Guard for the device. More...
|
| |
| int32_t | PN_setRtc3PortStatus (PRUICSS_HwAttrs const *pruicssHwAttrs, uint8_t portNumber, uint8_t status) |
| | API to set the RTClass3 port status of a port. More...
|
| |
| int32_t | PN_setStaticFilterTable (PRUICSS_HwAttrs const *pruicssHwAttrs, const uint8_t *macAddr, uint8_t ctrl, uint8_t portNumber, uint8_t table) |
| | API to enable/disable the reception & forward for a Multicast address in port multicast filter tables. More...
|
| |
| int32_t | PN_setWatchDogTimer (PN_Handle pnHandle, int32_t timerPeriod) |
| | API to configure the ICSS watchdog expiry duration. More...
|
| |
| int32_t | PN_loadStaticTable (PRUICSS_HwAttrs const *pruicssHwAttrs, const uint32_t *staticTable, uint8_t staticTableLength, uint8_t staticTableType, uint8_t portNumber) |
| | PN_loadStaticTable API to load multicast static table to ICSS memory. More...
|
| |
| void | PN_cpmIsrHandler (void *arg) |
| | Profinet CPM ISR handler. More...
|
| |
| void | PN_ppmIsrHandler (void *arg) |
| | Profinet PPM ISR handler. More...
|
| |
| void | PN_dhtIsrHandler (void *arg) |
| | Profinet DHT ISR handler. More...
|
| |
| void | PN_PTCP_isrHandler (void *arg) |
| | Profinet PTCP ISR handler. More...
|
| |
| void | PN_CPMOffloadBypass (PRUICSS_HwAttrs const *pruicssHwAttrs) |
| | API to configure the FW to store RTC1 CPM frames in Queue0 instead of CPM buffers. To be called by stack before the firmware load. More...
|
| |
| void | PN_storeIpAddress (PRUICSS_HwAttrs const *pruicssHwAttrs, const uint32_t devIpAddr) |
| | API to store current configured DUT IP address. More...
|
| |
| int32_t | PN_portFwdCtrl (PN_Handle pnHandle, uint8_t portNo, uint8_t portFwdState) |
| | API to configure port forwarding state. More...
|
| |