IO-Link Master2.02.04
 
Loading...
Searching...
No Matches
SMI Event

Overview

SMI Event.

Functions

IOL_FUNC_DECL IOL_EErrorType IOLM_SMI_eReportPortEvent (INT8U u8Port_p, IOL_EEType eEType_p, IOL_EEMode eEMode_p, INT16U u16ECode_p)
 Report port event.
 

Function Documentation

◆ IOLM_SMI_eReportPortEvent()

IOL_FUNC_DECL IOL_EErrorType IOLM_SMI_eReportPortEvent ( INT8U  u8Port_p,
IOL_EEType  eEType_p,
IOL_EEMode  eEMode_p,
INT16U  u16ECode_p 
)

Report port event.

This function can be used to report an application or profile specific port event.

Parameters
[in]u8Port_pPort ID.
[in]eEType_pEvent type.
[in]eEMode_pEvent mode.
[in]u16ECode_pEventCode.
Returns
Error