AM64x MCU+ SDK  11.00.00

Detailed Description

Ram driver configuration, these are filled by SysCfg based on the ram device that is selected.

Data Fields

Ram_Attrsattrs
 
Ram_Fxnsfxns
 
Ram_DevConfigdevConfig
 
void * object
 

Field Documentation

◆ attrs

Ram_Attrs* Ram_Config::attrs

Ram device attributes

◆ fxns

Ram_Fxns* Ram_Config::fxns

Ram device implementation functions

◆ devConfig

Ram_DevConfig* Ram_Config::devConfig

◆ object

void* Ram_Config::object

Ram driver object, used to maintain driver implementation state