Go to the source code of this file.
Data Structures | |
| struct | Config_Mem_Struct |
| struct | PRU_IPC_Attrs |
| struct | PRU_IPC_Params |
| struct | PRU_IPC_Object |
| struct | PRU_IPC_Config |
| This struct is used to store configurables for PRU_IPC. More... | |
Typedefs | |
| typedef struct PRU_IPC_Config_s * | PRU_IPC_Handle |
| A handle that is returned from a PRU_IPC_open() call. This handle is required for calling other PRU_IPC APIs. More... | |
| typedef void(* | PRU_IPC_CallbackFxn) (void *args) |
| A Callback function required to register callback on data receive if receive interrupt is enabled. More... | |
Functions | |
| void | PRU_IPC_init (void) |
| This function initializes the PRU_IPC module. More... | |
| void | PRU_IPC_deinit (void) |
| This function deinitializes the PRU_IPC module. More... | |
| void | PRU_IPC_Params_init (PRU_IPC_Params *params) |
| Function to set default values of PRU_IPC_Params in params. More... | |
| PRU_IPC_Handle | PRU_IPC_open (uint32_t idx, PRU_IPC_Params *params) |
| To initialize and configure PRU_IPC instance. More... | |
| void | PRU_IPC_close (PRU_IPC_Handle handle) |
| To stop/end PRU_IPC instance. More... | |
| uint16_t | PRU_IPC_getBlockId (PRU_IPC_Handle handle) |
| Reads the id of last written block by PRU from the PRU-Config memory. More... | |
| int32_t | PRU_IPC_getData (PRU_IPC_Handle handle, void *container) |
| Reads the data from the configured shared memory. More... | |
| int32_t | PRU_IPC_sendData (PRU_IPC_Handle handle, void *container) |
| Send/Write data to the configured shared memory (generates interrupt to PRU if it is enabled) More... | |