parameters to open the over IP mode raw socket, the values are in host order
Data Fields | |
uint32_t | laddr |
local IP address More... | |
uint16_t | lport |
local IP port More... | |
uint32_t | daddr |
destination IP address More... | |
uint16_t | dport |
destination IP port More... | |
uint32_t cb_rawsock_ovip_para_t::laddr |
local IP address
uint16_t cb_rawsock_ovip_para_t::lport |
local IP port
uint32_t cb_rawsock_ovip_para_t::daddr |
destination IP address
uint16_t cb_rawsock_ovip_para_t::dport |
destination IP port