AM64x MCU+ SDK  09.02.00
EnetPort_PriorityMap Struct Reference

Detailed Description

Priority map.

It can be used for priority regeneration as well as for QoS egress priority remapping.

Data Fields

uint32_t priorityMap [ENET_PRI_NUM]
 

Field Documentation

◆ priorityMap

uint32_t EnetPort_PriorityMap::priorityMap[ENET_PRI_NUM]

Packet priority map. Map index is the input priority, map value is the output priority.