Go to the source code of this file.
Macros | |
#define | SOC_BOOTMODE_MMCSD (0X36C3) |
Switch value for SD card boot mode. More... | |
#define | SOC_FWL_OPEN_MAGIC_NUM (0XFEDCBA98u) |
Software defined MAGIC number to indicate SRAM firewall open by SBL. More... | |
#define | MCU_MCSPI0_CFG_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_MCSPI0_CFG_BASE + 0x80000000) |
#define | MCU_MCSPI1_CFG_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_MCSPI1_CFG_BASE + 0x80000000) |
#define | MCU_UART0_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_UART0_BASE + 0x80000000) |
#define | MCU_UART1_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_UART1_BASE + 0x80000000) |
SOC Domain ID | |
#define | SOC_DOMAIN_ID_MAIN (0U) |
#define | SOC_DOMAIN_ID_MCU (1U) |
#define | SOC_PSC_DOMAIN_ID_MAIN (0U) |
#define | SOC_PSC_DOMAIN_ID_MCU (1U) |
SOC PSC Module State | |
#define | SOC_PSC_SYNCRESETDISABLE (0x0U) |
#define | SOC_PSC_SYNCRESET (0x1U) |
#define | SOC_PSC_DISABLE (0x2U) |
#define | SOC_PSC_ENABLE (0x3U) |
SOC PSC Domain State | |
#define | SOC_PSC_DOMAIN_OFF (0x0U) |
#define | SOC_PSC_DOMAIN_ON (0x1U) |
Functions | |
static int32_t | I2C_lld_isBaseAddrValid (uint32_t baseAddr) |
API to validate I2C base address. More... | |
static int32_t | MCSPI_lld_isBaseAddrValid (uint32_t baseAddr) |
API to validate MCSPI base address. More... | |
static int32_t | UART_IsBaseAddrValid (uint32_t baseAddr) |
API to validate UART base address. More... | |
int32_t | SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable) |
Enable clock to specified module. More... | |
int32_t | SOC_moduleSetClockFrequencyWithParent (uint32_t moduleId, uint32_t clkId, uint32_t clkParent, uint64_t clkRate) |
Set module clock to specified frequency and with a specific parent. More... | |
int32_t | SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate) |
Set module clock to specified frequency. More... | |
int32_t | SOC_moduleGetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t *clkRate) |
Get module clock frequency. More... | |
const char * | SOC_getCoreName (uint16_t coreId) |
Convert a core ID to a user readable name. More... | |
uint64_t | SOC_getSelfCpuClk (void) |
Get the clock frequency in Hz of the CPU on which the driver is running. More... | |
void | SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition) |
Lock control module partition to prevent writes into control MMRs. More... | |
void | SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition) |
Unlock control module partition to allow writes into control MMRs. More... | |
void | SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable) |
Enable or disable ePWM time base clock from Control MMR. More... | |
void | SOC_allowEpwmTzReg (uint32_t epwmInstance, uint32_t enable) |
Enable or disable writes to the EPWM tripZone registers. More... | |
uint64_t | SOC_virtToPhy (void *virtAddr) |
SOC Virtual (CPU) to Physical address translation function. More... | |
void * | SOC_phyToVirt (uint64_t phyAddr) |
Physical to Virtual (CPU) address translation function. More... | |
void | SOC_unlockAllMMR (void) |
Unlocks all the control MMRs. More... | |
void | SOC_setDevStat (uint32_t bootMode) |
Change boot mode by setting devstat register. More... | |
uint32_t | SOC_isR5FDualCoreMode (CSL_ArmR5CPUInfo *cpuInfo) |
Return R5SS supporting single or dual core mode. More... | |
void | SOC_generateSwWarmResetMainDomain (void) |
Generate SW Warm Reset Main Domain. More... | |
void | SOC_generateSwPORResetMainDomain (void) |
Generate SW POR Reset Main Domain. More... | |
uint32_t | SOC_getWarmResetCauseMainDomain (void) |
Get the reset reason source for Main Domain. More... | |
void | SOC_generateSwWarmResetMcuDomain (void) |
Generate SW WARM Reset Mcu Domain. More... | |
void | SOC_generateSwWarmResetMainDomainFromMcuDomain (void) |
Generate SW WARM Reset Main Domain from Mcu Domain. More... | |
void | SOC_generateSwPORResetMainDomainFromMcuDomain (void) |
Generate SW POR Reset Main Domain from Mcu Domain. More... | |
uint32_t | SOC_getWarmResetCauseMcuDomain (void) |
Get the reset reason source for Mcu Domain. More... | |
void | SOC_clearResetCauseMainMcuDomain (uint32_t resetCause) |
Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLMMR_MCU_RST_SRC register. It is read only. So we need to write 1 to CTRLMMR_MCU_RST_SRC to clear the reset reason. More... | |
int32_t | SOC_enableResetIsolation (uint32_t main2McuIsolation, uint32_t mcu2MainIsolation, uint32_t debugIsolationEnable) |
Enable reset isolation of MCU domain for safety applications. More... | |
void | SOC_setMCUResetIsolationDone (uint32_t value) |
Set MCU reset isolation done flag. More... | |
void | SOC_waitMainDomainReset (void) |
Wait for main domain reset to complete. More... | |
int32_t | SOC_getPSCState (uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t *domainState, uint32_t *moduleState) |
Get PSC (Power Sleep Controller) state. More... | |
int32_t | SOC_setPSCState (uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t pscState) |
Set PSC (Power Sleep Controller) state. More... | |
void | SOC_waitForFwlUnlock (void) |
Wait for Firewall unlock from SBL. The function polls for a Software defined Magic number at the PSRAM location (Software defined) More... | |
int32_t | SOC_isHsDevice (void) |
Check the device is HS or not. More... | |
uint32_t | SOC_getFlashDataBaseAddr (void) |
This function gets the SOC mapped data base address of the flash. More... | |