AM64x MCU+ SDK  09.02.00

Introduction

Functions

Functions

int32_t SDL_MTOG_init (SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
 Initialize Master TOG module with respect of instance. More...
 
int32_t SDL_MTOG_verifyConfig (SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
 Verifying written configuration with Master TOG module. More...
 
int32_t SDL_MTOG_start (SDL_MTOG_Inst instance)
 Start the timeout function. More...
 
int32_t SDL_MTOG_stop (SDL_MTOG_Inst instance)
 Stop the timeout function. More...
 
int32_t SDL_MTOG_forceTimeout (SDL_MTOG_Inst instance)
 Force a timeout. More...
 
int32_t SDL_MTOG_reset (SDL_MTOG_Inst instance)
 Reset the timeout functionality. More...
 
int32_t SDL_MTOG_getStaticRegisters (SDL_MTOG_Inst instance, SDL_MTOG_staticRegs *pStaticRegs)
 Readback Static configuration register. More...
 

Function Documentation

◆ SDL_MTOG_init()

int32_t SDL_MTOG_init ( SDL_MTOG_Inst  instance,
const SDL_MTOG_config pConfig 
)

Initialize Master TOG module with respect of instance.

This function allows software to initialize MTOG module

The pConfig contains the timeout value

Parameters
instance[IN] MTOG instance
pConfig[IN] Pointer to store the configuration
Returns
SDL_PASS The function completed successfully SDL_EBADARGS instance is invalid or pConfig is NULL

◆ SDL_MTOG_verifyConfig()

int32_t SDL_MTOG_verifyConfig ( SDL_MTOG_Inst  instance,
const SDL_MTOG_config pConfig 
)

Verifying written configuration with Master TOG module.

This function allows software to verifying MTOG module

The pConfig contains the timeout value

Parameters
instance[IN] MTOG instance
pConfig[IN] Pointer to store the configuration
Returns
SDL_PASS The function completed successfully SDL_EBADARGS instance is invalid or pConfig is NULL

◆ SDL_MTOG_start()

int32_t SDL_MTOG_start ( SDL_MTOG_Inst  instance)

Start the timeout function.

This function starts the timeout counter functionality.

Parameters
instance[IN] MTOG instance
Returns
SDL_PASS Function completed successfully SDL_EBADARGS pRegs is NULL

◆ SDL_MTOG_stop()

int32_t SDL_MTOG_stop ( SDL_MTOG_Inst  instance)

Stop the timeout function.

This function stops the timeout counter functionality.

Parameters
instance[IN] MTOG instance
Returns
SDL_PASS Function completed successfully SDL_EBADARGS pRegs is NULL

◆ SDL_MTOG_forceTimeout()

int32_t SDL_MTOG_forceTimeout ( SDL_MTOG_Inst  instance)

Force a timeout.

This function enables software to force a timeout and flush of the interface transactions.

Parameters
instance[IN] MTOG instance
Returns
SDL_PASS Function completed successfully SDL_EFAIL Timeout function is disabled. Call SDL_MTOG_start first. SDL_EBADARGS pRegs is NULL

◆ SDL_MTOG_reset()

int32_t SDL_MTOG_reset ( SDL_MTOG_Inst  instance)

Reset the timeout functionality.

This function resets the timeout functionality by clearing the timeout interrupt and timeout counter. It should be called after servicing a timeout interrupt and before re-enabling the timeout counter via the SDL_MTOG_start function.

Note that the timeout value set via the SDL_MTOG_setTimeoutVal function is unaffected.

Parameters
instance[IN] MTOG instance
Returns
SDL_PASS Function completed successfully SDL_EBADARGS pRegs is NULL

◆ SDL_MTOG_getStaticRegisters()

int32_t SDL_MTOG_getStaticRegisters ( SDL_MTOG_Inst  instance,
SDL_MTOG_staticRegs pStaticRegs 
)

Readback Static configuration register.

This function reads back configuration registers that are static. Note that this is just one register master TOG

Parameters
instance[IN] MTOG instance
pStaticRegs[OUT] Pointer to store the read static registers
Returns
SDL_PASS Function completed successfully SDL_EBADARGS pRegs is NULL