AM64x MCU+ SDK  09.02.00
enet_utils_dflt.h File Reference

Introduction

This file contains the type definitions and function prototypes of the Enet Utils default implementation.

Go to the source code of this file.

Functions

void EnetUtilsDflt_initCfg (EnetUtils_Cfg *cfg)
 Initialize EnetUtils config with default parameters. More...
 

Function Documentation

◆ EnetUtilsDflt_initCfg()

void EnetUtilsDflt_initCfg ( EnetUtils_Cfg cfg)

Initialize EnetUtils config with default parameters.

Initializes the EnetUtils config parameters with default ones: PDK UART-based printf and one-to-one virtual-to-physical and physical-to-virtual memory translation functins.

Parameters
cfgPointer to the initialization parameters to be initialized