AM64x INDUSTRIAL COMMUNICATIONS SDK  09.02.00
lastActiveNode Struct Reference

Detailed Description

Last active node at the end of the chain Class for Attributes 6 and 7.

Data Fields

uint32_t ipAddr
 
uint8_t macAddr [6]
 
uint16_t deviceNum
 

Field Documentation

◆ ipAddr

uint32_t lastActiveNode::ipAddr

IP Address of the last active Node

◆ macAddr

uint8_t lastActiveNode::macAddr[6]

MAC of the last node

◆ deviceNum

uint16_t lastActiveNode::deviceNum

from 0-N where N is the number of nodes (excluding supervisor) in the ring