AM64x INDUSTRIAL COMMUNICATIONS SDK  09.02.00

Introduction

Functions

void bsp_set_digio_sw_dataout_enable (PRUICSS_Handle pruIcssHandle)
 Configure digio for sw controlled dataout mode. More...
 
void bsp_set_digio_out (PRUICSS_Handle pruIcssHandle, uint8_t num)
 Set selected digital output pin. More...
 
void bsp_clear_digio_out (PRUICSS_Handle pruIcssHandle, uint8_t num)
 Clear selected digital output pin. More...
 

Function Documentation

◆ bsp_set_digio_sw_dataout_enable()

void bsp_set_digio_sw_dataout_enable ( PRUICSS_Handle  pruIcssHandle)

Configure digio for sw controlled dataout mode.

Parameters
pruIcssHandlePRUSS Handle

◆ bsp_set_digio_out()

void bsp_set_digio_out ( PRUICSS_Handle  pruIcssHandle,
uint8_t  num 
)

Set selected digital output pin.

Parameters
pruIcssHandlePRUSS Handle
numdigital output selection (num =0 to 7)

◆ bsp_clear_digio_out()

void bsp_clear_digio_out ( PRUICSS_Handle  pruIcssHandle,
uint8_t  num 
)

Clear selected digital output pin.

Parameters
pruIcssHandlePRUSS Handle
numdigital output selection (num =0 to 7)