AM64x MCU+ SDK  09.01.00
tisci_bitops.h File Reference

Go to the source code of this file.

Macros

#define TISCI_BIT(n)   (((uint32_t) 1U) << (n))
 This file contains: More...
 

Functions

static uint32_t get_field (uint32_t val, uint32_t end, uint32_t start)
 extract the specified bit field from a 32 bit unsigned integer. More...
 
static uint32_t set_field (uint32_t tgt, uint32_t end, uint32_t start, uint32_t val)
 set the specified bit field from a 32 bit unsigned integer to provided value More...
 
static uint32_t get_mask (uint32_t end, uint32_t start)
 Generate a mask for the give bit field [end:start]. More...