AM64x MCU+ SDK  09.01.00
sockaddr Struct Reference

Detailed Description

Structure representing the lld_sockaddr instance.

Data Fields

unsigned char sll_addr [6]
 
int macport
 
int tcid
 

Field Documentation

◆ sll_addr

unsigned char sockaddr::sll_addr[6]

Source MAC address of the socket.

◆ macport

int sockaddr::macport

MAC port number.

◆ tcid

int sockaddr::tcid

Traffic class ID. Valid values start from 0. Set to -1 to use the default assigned by the implementation.