AM64x MCU+ SDK  09.01.00
SDL_VTM_staticRegsTs Struct Reference

Detailed Description

VTM Static Registers for Temperature sensor.

This structure contains VTM static register for a given configuration The register values are not expected to change until a new configuration is done.

Data Fields

uint32_t vtm_ts_ctrl2
 
uint32_t vtm_ts_ctrl
 
uint32_t vtm_ts_th
 
uint32_t vtm_ts_th2
 

Field Documentation

◆ vtm_ts_ctrl2

uint32_t SDL_VTM_staticRegsTs::vtm_ts_ctrl2

VTM individual sensor cfg2 control information

◆ vtm_ts_ctrl

uint32_t SDL_VTM_staticRegsTs::vtm_ts_ctrl

VTM individual sensor cfg1 control information

◆ vtm_ts_th

uint32_t SDL_VTM_staticRegsTs::vtm_ts_th

VTM individual sensor threshold information

◆ vtm_ts_th2

uint32_t SDL_VTM_staticRegsTs::vtm_ts_th2

VTM individual sensor threshold2 information