AM64x MCU+ SDK  09.01.00

Detailed Description

Firewall atributes.

Firewall attributes are used within Firewall_open(). The attributes are used to initialize Firewall ID MMR as per the attributes

Data Fields

uint32_t firewallId
 
uint32_t totalRegions
 
uint32_t initRegions
 
Firewall_RegionCfgregionInfo
 

Field Documentation

◆ firewallId

uint32_t Firewall_Attrs::firewallId

◆ totalRegions

uint32_t Firewall_Attrs::totalRegions

◆ initRegions

uint32_t Firewall_Attrs::initRegions

◆ regionInfo

Firewall_RegionCfg* Firewall_Attrs::regionInfo