AM64x MCU+ SDK  09.01.00
CSL_UdmapTdResponse Struct Reference

Data Fields

uint32_t tdIndicator
 
uint32_t chId
 
uint32_t forced
 

Field Documentation

◆ tdIndicator

uint32_t CSL_UdmapTdResponse::tdIndicator

TRUE: Indicates that a teardown has completed.

◆ chId

uint32_t CSL_UdmapTdResponse::chId

Indicates which channel the teardown completed on.

◆ forced

uint32_t CSL_UdmapTdResponse::forced

FALSE: Indicates that the teardown was graceful and data was not lost. TRUE : Indicates that the teardown was not graceful and data was potentially lost