AM64x MCU+ SDK  09.01.00
sdl_mtog.h File Reference

Go to the source code of this file.

Data Structures

struct  SDL_MTOG_staticRegs
 Master TOG Static Registers. More...
 
struct  SDL_MTOG_config
 

Macros

#define SDL_MTOG_FORCE_KEY   ((uint32_t) 0x95U)
 

Functions

int32_t SDL_MTOG_init (SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
 Initialize Master TOG module with respect of instance. More...
 
int32_t SDL_MTOG_verifyConfig (SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
 Verifying written configuration with Master TOG module. More...
 
int32_t SDL_MTOG_start (SDL_MTOG_Inst instance)
 Start the timeout function. More...
 
int32_t SDL_MTOG_stop (SDL_MTOG_Inst instance)
 Stop the timeout function. More...
 
int32_t SDL_MTOG_forceTimeout (SDL_MTOG_Inst instance)
 Force a timeout. More...
 
int32_t SDL_MTOG_reset (SDL_MTOG_Inst instance)
 Reset the timeout functionality. More...
 
int32_t SDL_MTOG_getStaticRegisters (SDL_MTOG_Inst instance, SDL_MTOG_staticRegs *pStaticRegs)
 Readback Static configuration register. More...
 

Macro Definition Documentation

◆ SDL_MTOG_FORCE_KEY

#define SDL_MTOG_FORCE_KEY   ((uint32_t) 0x95U)