AM64x INDUSTRIAL COMMUNICATIONS SDK  09.01.00
exceptionList Struct Reference

Detailed Description

List of MAC ID's which are exempted from Learning, this is for DLR implementation.

Data Fields

uint8_t MAC [6]
 
uint8_t numExceptions
 

Field Documentation

◆ MAC

uint8_t exceptionList::MAC[6]

MAC ID of supervisor which is exempt from learning

◆ numExceptions

uint8_t exceptionList::numExceptions

number of exceptions, this is a flag where value greater than 1 indicates that exception exists