AM64x INDUSTRIAL COMMUNICATIONS SDK  09.01.00
TLV1_TAG Struct Reference

Detailed Description

TLV1 tag

Data Fields

uint8_t type
 
uint8_t mac_length
 
uint8_t dan_mac [ETHER_ADDR_LEN]
 

Field Documentation

◆ type

uint8_t TLV1_TAG::type

Indicates the HSR node in normal operation or PRP node in Duplicate Discard or Accept

◆ mac_length

uint8_t TLV1_TAG::mac_length

Length of the following MAC address in octets

◆ dan_mac

uint8_t TLV1_TAG::dan_mac[ETHER_ADDR_LEN]

MAC address used by the sender