AM263x MCU+ SDK  09.02.00
networking/enet/core/include/mod/mdio.h File Reference

Introduction

This file contains the type definitions and helper macros for the MDIO module interface.

Go to the source code of this file.

Data Structures

struct  Mdio_Cfg
 MDIO module configuration. More...
 

Macros

#define MDIO_MAX_PHY_CNT   (31U)
 Maximum number of PHYs supported on MDIO bus. More...
 

Enumerations

enum  Mdio_OpMode { MDIO_MODE_NORMAL = 0U, MDIO_MODE_STATE_CHANGE_MON, MDIO_MODE_MANUAL }
 MDIO operating mode. More...
 

Functions

void Mdio_initCfg (Mdio_Cfg *mdioCfg)
 Initialize MDIO configuration parameters. More...