AM263x MCU+ SDK  09.00.00
APIs for DTHE AES

Introduction

This module contains APIs to program and use the DTHE AES.

Files

file  dthe_aes.h
 This file contains the prototype of DTHE AES driver APIs.
 

Data Structures

struct  DTHE_AES_Params
 AES Driver Parameters This structure has all the parameters which are need by the AES Driver to perform the specified operation. More...
 

Functions

DTHE_AES_Return_t DTHE_AES_open (DTHE_Handle handle)
 Function to Open DTHE AES Driver. More...
 
DTHE_AES_Return_t DTHE_AES_execute (DTHE_Handle handle, const DTHE_AES_Params *ptrParams)
 The function is used to execute the AES Driver with the specified parameters. More...
 
DTHE_AES_Return_t DTHE_AES_close (DTHE_Handle handle)
 Function to close DTHE AES Driver. More...
 

Enumerations

enum  DTHE_AES_Return_t { DTHE_AES_RETURN_SUCCESS = 0x62E699D9U, DTHE_AES_RETURN_FAILURE = 0x904D041AU }
 DTHE AES Driver Error code. More...
 

Macros

#define DTHE_AES_ECB_MODE   (0x00000000U)
 Flag for AEC ECB Mode. More...
 
#define DTHE_AES_CBC_MODE   (0x00000001U)
 Flag for AEC CBC Mode. More...
 
#define DTHE_AES_KEY_128_SIZE   (0x00000001U)
 Size of AES key is of 128-bit. More...
 
#define DTHE_AES_KEY_192_SIZE   (0x00000002U)
 Size of AES key is of 192-bit. More...
 
#define DTHE_AES_KEY_256_SIZE   (0x00000003U)
 Size of AES key is of 256-bit. More...
 
#define DTHE_AES_ENCRYPT   (0x016FE45DU)
 AES Encrypt Flag. More...
 
#define DTHE_AES_DECRYPT   (0xDCBA4213U)
 AES Decrypt Flag. More...
 

Macro Definition Documentation

◆ DTHE_AES_ECB_MODE

#define DTHE_AES_ECB_MODE   (0x00000000U)

Flag for AEC ECB Mode.

◆ DTHE_AES_CBC_MODE

#define DTHE_AES_CBC_MODE   (0x00000001U)

Flag for AEC CBC Mode.

◆ DTHE_AES_KEY_128_SIZE

#define DTHE_AES_KEY_128_SIZE   (0x00000001U)

Size of AES key is of 128-bit.

◆ DTHE_AES_KEY_192_SIZE

#define DTHE_AES_KEY_192_SIZE   (0x00000002U)

Size of AES key is of 192-bit.

◆ DTHE_AES_KEY_256_SIZE

#define DTHE_AES_KEY_256_SIZE   (0x00000003U)

Size of AES key is of 256-bit.

◆ DTHE_AES_ENCRYPT

#define DTHE_AES_ENCRYPT   (0x016FE45DU)

AES Encrypt Flag.

◆ DTHE_AES_DECRYPT

#define DTHE_AES_DECRYPT   (0xDCBA4213U)

AES Decrypt Flag.

Enumeration Type Documentation

◆ DTHE_AES_Return_t

DTHE AES Driver Error code.

The enumeration describes all the possible return and error codes which the DTHE AES Driver can return

Enumerator
DTHE_AES_RETURN_SUCCESS 

Success/pass return code

DTHE_AES_RETURN_FAILURE 

General or unspecified failure/error

Function Documentation

◆ DTHE_AES_open()

DTHE_AES_Return_t DTHE_AES_open ( DTHE_Handle  handle)

Function to Open DTHE AES Driver.

Parameters
handleDTHE_Handle returned from DTHE_open().
Returns
DTHE_AES_RETURN_SUCCESS if requested operation completed. DTHE_AES_RETURN_FAILURE if requested operation not completed.

◆ DTHE_AES_execute()

DTHE_AES_Return_t DTHE_AES_execute ( DTHE_Handle  handle,
const DTHE_AES_Params ptrParams 
)

The function is used to execute the AES Driver with the specified parameters.

Parameters
handleDTHE_Handle returned from DTHE_open().
ptrParamsPointer to the parameters to be used to execute the driver.
Returns
DTHE_AES_RETURN_SUCCESS if requested operation completed. DTHE_AES_RETURN_FAILURE if requested operation not completed.

◆ DTHE_AES_close()

DTHE_AES_Return_t DTHE_AES_close ( DTHE_Handle  handle)

Function to close DTHE AES Driver.

Parameters
handleDTHE_Handle returned from DTHE_open().
Returns
DTHE_AES_RETURN_SUCCESS if requested operation completed. DTHE_AES_RETURN_FAILURE if requested operation not completed.